cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H743x: Start new project now? Availability forecast?

Torsten Aurich
Associate II
Posted on October 16, 2017 at 11:05

Dear ST-Team,

for our new project we plan to use STM32H743x. We plan to go into HW-Design Q4-2017

and start FW-Design end of 2017. Regarding this i have some questions with the use

of the H7-Devices:

1. We want to buy a Nucleo-H743ZI. Which die revision are on these boards? Which limitation

does have the chip respectively which errata sheet revision is true?

2. Beside the core for our app the following peripheral components are importent:

- ETH (RMII)

- I2C

- RCC

- SDMMC (SDIO 4Bits Wide Bus 50MHz)

- SPI (Full Duplex Master)

- SYS (SWD)

- some Timers

- USB-OTG-FS

- USB-OTG-HS (with ULPI-Phy)

Would you say it is uncritical to start HW- and FW-Design because end of 2017 there are

a H7-derivative on the market available, which fulfils a correct operation with all these

peripherals? And if yes, tell me please the chip part number.

Thanx in advance!!!

Regards

TA

##stm32h7
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
AvaTar
Lead
Posted on October 16, 2017 at 12:11

Dear ST-Team,

...

Would you say it is uncritical to start HW- and FW-Design because end of 2017 there are

a H7-derivative on the market available, which fulfils a correct operation with all these

peripherals? And if yes, tell me please the chip part number.

There seems to be a small misunderstanding.

This is a public forum, with many volunteers not affiliated with ST (say, customers & users) - and some ST staff.

But I doubt ST will publish future plans here, or talk about silicon issues in depth ...

I suggest to contact a ST FAE, or a local distributor directly.

Cedric LECOUTRE
ST Employee
Posted on October 17, 2017 at 18:51

Hi

torsten.aurich

‌,

On current

http://www.st.com/content/st_com/en/products/evaluation-tools/product-evaluation-tools/mcu-eval-tools/stm32-mcu-eval-tools/stm32-mcu-nucleo/nucleo-h743zi.html

, you will find a

http://www.st.com/content/st_com/en/products/microcontrollers/stm32-32-bit-arm-cortex-mcus/stm32-high-performance-mcus/stm32h7-series/stm32h7x3/stm32h743zi.html

rev. Y. So you can fully rely on the errata sheet

http://www.st.com/resource/en/errata_sheet/dm003684pdf

to understand its limitations.In this document, you will also be able to checkstatus of these limitations for next MCU revision.

About exact availability date of theserevisions,

meyer.frank

‌ is right, it is better to contactus through

https://my.st.com/content/my_st_com/en/support/online-support.html

. Nevertheless, I think that with the peripherals you have listed, you can start working with current revision: and if you want to access to SDMMC, ETH and USB OTG HS, you might as well use a

http://www.st.com/content/st_com/en/products/evaluation-tools/product-evaluation-tools/mcu-eval-tools/stm32-mcu-eval-tools/stm32-mcu-eval-boards/stm32h743i-eval.html

for development.

Best regards,

Cédric

Torsten Aurich
Associate II
Posted on October 18, 2017 at 08:31

Hi Guys,

thank you very much for the information.

Kind Regards

Torsten

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.