2022-04-01 2:02 PM
Hi,
Is SDRAM over FMC supported in STM32H743VIT6 MCUs? I can't see this option in CubeMX, only NOR Flash/PSRAM/SRAM/ROM/LCD and NAND Flash. The datasheet says that SDRAM is not supported in LQFP144 packages, but my one is LQFP100.
Looking forward for any help.
2022-04-01 2:15 PM
Even fewer pins, so assuming more of the pins you'd need are absent...
Try the Data Sheet and then play Pin Bingo
2022-04-01 2:30 PM
FMC_SDNRAS, FMC_SDNCAS ?
2022-04-01 5:34 PM
SDRAM is not available on the LQFP100 either. FMC_A0, among many others, is absent on the pinout.
2022-04-02 9:16 AM
Thank you very much Tesla and TDK. I have checked the pinout once more and now I see that some necessary pins for SDRAM support are absent in LQFP100 package. It's a pity.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.