2022-01-05 4:52 AM
I'm stock since a while now.
I use H723 nucleo board with a SD card socket, build for SPI, but I use it as SDMMC with 1bit wide.
this socket is ok with SD and SPI.
f_mount send FR_NOT_READY.
I have the same answer with or with out Sd card...
I use a logic analyser and I can see that the clock never stop after start
is anybody have a clue or a simple working project with H723 and SDMMC ?
Solved! Go to Solution.
2022-01-10 7:30 AM
It's working now, I make a(classic) mistakes : sd detection !
2022-01-10 7:30 AM
It's working now, I make a(classic) mistakes : sd detection !
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.