2025-04-22 9:05 AM - last edited on 2025-04-22 9:20 AM by mƎALLEm
I have a Nucleo-H723ZG board. The GPIO lock bits are set at reset so I cannot set up the ports. See Attached screenshot. I can run code just fine and the original demo code did toggle the LEDs.
Am I missing something here?
Solved! Go to Solution.
2025-04-22 2:22 PM
> all of the GPIOA registers report 0xABFFFFFF
That's sign of GPIOA clock not being enabled in RCC.
JW
2025-04-22 9:22 AM
Since all of the GPIOA registers report 0xABFFFFFF, I'm more inclined to believe this is a debugger/IDE issue.
2025-04-22 9:24 AM
Hello @Niramas and welcome to the ST community,
I'm confused. You said:
@Niramas wrote:
I can run code just fine and the original demo code did toggle the LEDs.
The LEDs are toggling even the lock bits are set after reset?
2025-04-22 11:08 AM
The screenshot is not from the demo it is from our SW. Notice it is stopped at the reset vector though.
2025-04-22 11:09 AM
The demo came pre loaded on the device and is gone now.
2025-04-22 11:10 AM
The memory dump shows the same values.
2025-04-22 2:22 PM
> all of the GPIOA registers report 0xABFFFFFF
That's sign of GPIOA clock not being enabled in RCC.
JW
2025-04-22 2:44 PM
I had always thought GPIOA clock was required to be enabled for SWD to be active and was therefore enabled by default. Testing it now, it clearly (a) isn't enabled by default and (b) doesn't need to be enabled for SWD to work.
2025-04-22 2:49 PM
But the docs say the Locks are reset at reset without any mention of the clock.
2025-04-22 2:50 PM
Are you saying they may be actually correct but the debugger can't read them because the clock is off?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.