2023-07-26 8:50 PM
Im moving my project code from stmf407 to stm32h743 and i have stucked with spi. First of all stmh743 has many more registers and it also lack some of them like RXONLY register in CR1. What im trying to do its receive 19bytes from the master,the master is a complete device and i cant control it. The clock speed of the master is around 20nanoseconds. My previous project in stmf407 catching the data perfectly.
working STM32F407 spi code:
static void MX_SPI1_Init(void)
{
SPI1 parameter configuration*/
hspi1.Instance = SPI1;
hspi1.Init.Mode = SPI_MODE_SLAVE;
hspi1.Init.Direction = SPI_DIRECTION_2LINES_RXONLY;
hspi1.Init.DataSize = SPI_DATASIZE_8BIT;
hspi1.Init.CLKPolarity = SPI_POLARITY_LOW;
hspi1.Init.CLKPhase = SPI_PHASE_1EDGE;
hspi1.Init.NSS = SPI_NSS_SOFT;
hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;
hspi1.Init.TIMode = SPI_TIMODE_DISABLE;
hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
hspi1.Init.CRCPolynomial = 10;
if (HAL_SPI_Init(&hspi1) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
}
static void ReadSpi(void)
{
RxSPI1 = 0;
MX_SPI1_Init();
GPIOA->MODER = 0xAA809910;
SPI1->CR1 |= 0x40;
RxCounter = 0;
while(RxCounter <20){
while (!(hspi1.Instance->SR & SPI_FLAG_RXNE))
;
RxSPI = hspi1.Instance->DR;
// now you have 8 SPI clock cycles to do something with the data
if (RxSPI != 0xFF )
{
RxTable[RxCounter++] = RxSPI;
}
}
return;
}
STM32H743 CODE:
static void ReadSpi(void)
{
RxSPI1 = 0;
MX_SPI1_Init();
GPIOA->MODER = 0xAA809910;
SPI1->CR1 |= SPI_CFG2_SSM;
SPI1->CR1 |= SPI_CR1_SSI;
SPI1->CR1 |= SPI_CR1_SPE;
RxCounter = 0;
while(RxCounter <20){
while (!(hspi1.Instance->SR & SPI_FLAG_RXP))
;
RxSPI = hspi1.Instance->RXDR;
// now you have 8 SPI clock cycles to do something with the data
if (RxSPI != 0xFF )
{
RxTable[RxCounter++] = RxSPI;
}
}
return;
}
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Supply configuration update enable
*/
HAL_PWREx_ConfigSupply(PWR_LDO_SUPPLY);
/** Configure the main internal regulator output voltage
*/
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE3);
while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {}
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL.PLLM = 1;
RCC_OscInitStruct.PLL.PLLN = 24;
RCC_OscInitStruct.PLL.PLLP = 2;
RCC_OscInitStruct.PLL.PLLQ = 4;
RCC_OscInitStruct.PLL.PLLR = 2;
RCC_OscInitStruct.PLL.PLLRGE = RCC_PLL1VCIRANGE_3;
RCC_OscInitStruct.PLL.PLLVCOSEL = RCC_PLL1VCOWIDE;
RCC_OscInitStruct.PLL.PLLFRACN = 0;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
|RCC_CLOCKTYPE_D3PCLK1|RCC_CLOCKTYPE_D1PCLK1;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV1;
RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV1;
RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)
{
Error_Handler();
}
}
static void MX_SPI1_Init(void)
{
hspi1.Instance = SPI1;
hspi1.Init.Mode = SPI_MODE_SLAVE;
hspi1.Init.Direction = SPI_DIRECTION_2LINES_RXONLY;
hspi1.Init.DataSize = SPI_DATASIZE_8BIT;
hspi1.Init.CLKPolarity = SPI_POLARITY_LOW;
hspi1.Init.CLKPhase = SPI_PHASE_1EDGE;
hspi1.Init.NSS = SPI_NSS_SOFT;
hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;
hspi1.Init.TIMode = SPI_TIMODE_DISABLE;
hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
hspi1.Init.CRCPolynomial = 0x0;
hspi1.Init.NSSPMode = SPI_NSS_PULSE_DISABLE;
hspi1.Init.NSSPolarity = SPI_NSS_POLARITY_LOW;
hspi1.Init.FifoThreshold = SPI_FIFO_THRESHOLD_01DATA;
hspi1.Init.TxCRCInitializationPattern = SPI_CRC_INITIALIZATION_ALL_ZERO_PATTERN;
hspi1.Init.RxCRCInitializationPattern = SPI_CRC_INITIALIZATION_ALL_ZERO_PATTERN;
hspi1.Init.MasterSSIdleness = SPI_MASTER_SS_IDLENESS_00CYCLE;
hspi1.Init.MasterInterDataIdleness = SPI_MASTER_INTERDATA_IDLENESS_00CYCLE;
hspi1.Init.MasterReceiverAutoSusp = SPI_MASTER_RX_AUTOSUSP_DISABLE;
hspi1.Init.MasterKeepIOState = SPI_MASTER_KEEP_IO_STATE_DISABLE;
hspi1.Init.IOSwap = SPI_IO_SWAP_DISABLE;
if (HAL_SPI_Init(&hspi1) != HAL_OK)
{
Error_Handler();
}
}
What im catching:
So i have a hard time to make spi of stm32h743 work as same as stm32f407's spi
line where we are waiting before catch the data in stm32f4 is while (!(hspi1.Instance->SR & SPI_FLAG_RXNE))
and in stm32h743: while (!(hspi1.Instance->SR & SPI_FLAG_RXP)) the flag names are diffrent but i gues its ok. here is imahge of initialized registers of noth mcus in the debug mode.
STM32f407:
STM32H743:
as you can see stm32h7 has a lot if registers i didnt met before like FIFO and CSUPS etc... and lack of crucial registers as RXONLY.
f4 working fine, while h7 have around 4-6(rxcounter equls 4-6 and then it just hangs) interaction with:
while(RxCounter <20){ while (!(hspi1.Instance->SR & SPI_FLAG_RXP)) ; RxSPI = hspi1.Instance->RXDR; // now you have 8 SPI clock cycles to do something with the data if (RxSPI != 0xFF ) { RxTable[RxCounter++] = RxSPI; } } return; }
I have tried a lot to make it work, seems like nothing working. I started to think that the problem with clock freq, can it be so?
here is clock configuration of STMH743:
here is clock configuration of STMf407:
as you can see stmf4 has a higher clock, can it be the issue?
Solved! Go to Solution.
2023-08-03 3:15 AM
the thing is that SPI never worked for me in stm32h743, it is stm32F407 spi working perfect and from it im trying to migrate the code in H7. Im trying to read from the same Master for both, so H7 just cant accomplish it
the strange thing is that H7 counting rxcounter 4-14 times and it means that
while (!(hspi1.Instance->SR & SPI_FLAG_RXNE))catches some data, right?
but
RxTable[30] is empty most of the times, rarely it catches frist byte with 0x40 value( strange value)so i cant understand where the problem is, its either catching flag wrong or reading
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.