2018-04-06 7:43 AM
Hai, Iam using the STM32H743VIT controller , We are using the spi4 in our board ,we generated the code using the cube mx nothing is coming(CLK and SIN)when transmit the data using the function ( HAL_SPI_Transmit(SPI_HandleTypeDef *hspi, uint8_t *pData, uint16_t Size, uint32_t Timeout)). we configured the SPI to the 8 bit mode.But with the same configuration the SPI2 is working fine.
Thank you
Best regards
Maheshwar.
#uphill-skiing #stm32h7-spi-sync #stm32h7 #spi Note: this post was migrated and contained many threaded conversations, some content may be missing.Solved! Go to Solution.
2019-01-02 7:59 AM
Is there any progress of this issue?
Maybe I have the same problem:
https://community.st.com/s/question/0D50X0000AAI2pESQT/stm32h743ii-spidma-malfunction
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.