2021-04-01 7:24 AM
Hello everyone;
I'm working LUPART with STM32H747. I have a problem like this;
- LPUART 1000000 baudRate has been installed. LSE clock is not used.
There is no problem when the LPUART's RX-TX line is physically connected to the module. But when I physically remove the module, the processor does not execute the code at runtime. Constantly getting stuck in LPUART1_IRQHandler function. The problem disappears when I drop the BaudRate for example 9600. Below is the interrupt routine I wrote for LPUART. It works smoothly on all other UART / USARTs.
static void DS_LPUSART1_InterruptCallback(UART_HandleTypeDef *huart)
{
uint32_t isrflags = READ_REG(huart->Instance->ISR);
uint32_t cr1its = READ_REG(huart->Instance->CR1);
uint32_t cr3its = READ_REG(huart->Instance->CR3);
uint8_t received_data = 0;
bool is_transmit_in_progress = false;
if ( ( (isrflags & USART_ISR_RXNE_RXFNE) != 0U) &&
( ( (cr1its & USART_CR1_RXNEIE_RXFNEIE) != 0U) ||
( (cr3its & USART_CR3_RXFTIE) != 0U)
)
)
{
received_data = (uint8_t) READ_REG(huart->Instance->RDR);
lpuart1.receiveByte(received_data);
}
if ( ( (isrflags & USART_ISR_TXE_TXFNF) != 0U) &&
( ( (cr1its & USART_CR1_TXEIE_TXFNFIE) != 0U) ||
( (cr3its & USART_CR3_TXFTIE) != 0U)
)
)
{
is_transmit_in_progress = lpuart1.transmit();
if(is_transmit_in_progress == false)
{
CLEAR_BIT(huart->Instance->CR1, USART_CR1_TXEIE_TXFNFIE);
}
}
}
void initialize(void)
{
static uint8_t dummy = 0;
uart_handle->pRxBuffPtr = &dummy;
uart_handle->RxXferSize = 1;
uart_handle->RxXferCount = 1;
uart_handle->ErrorCode = HAL_UART_ERROR_NONE;
SET_BIT(uart_handle->Instance->CR3, USART_CR3_EIE);
SET_BIT(uart_handle->Instance->CR1, USART_CR1_PEIE | USART_CR1_RXNEIE_RXFNEIE);
CLEAR_BIT(uart_handle->Instance->ISR,USART_ISR_NE);
switch(uart_number)
{
case uart_module_type::H747_LPUART1 :
uart_handle->RxISR = DS_LPUSART1_InterruptCallback; ///< While interrupt routines are init, they are handled to ISR registers.
uart_handle->TxISR = DS_LPUSART1_InterruptCallback; ///< While interrupt routines are init, they are handled to ISR registers.
break;
default :
//Error
break;
}
}Below is the initialize funciton I wrote for LPUART.
void MX_LPUART1_UART_Init(void)
{
hlpuart1.Instance = LPUART1;
hlpuart1.Init.BaudRate = 100000;
hlpuart1.Init.WordLength = UART_WORDLENGTH_9B;
hlpuart1.Init.StopBits = UART_STOPBITS_2;
hlpuart1.Init.Parity = UART_PARITY_EVEN;
hlpuart1.Init.Mode = UART_MODE_TX_RX;
hlpuart1.Init.HwFlowCtl = UART_HWCONTROL_NONE;
hlpuart1.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
hlpuart1.Init.ClockPrescaler = UART_PRESCALER_DIV1;
hlpuart1.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_TXINVERT_INIT|UART_ADVFEATURE_RXINVERT_INIT;
hlpuart1.AdvancedInit.TxPinLevelInvert = UART_ADVFEATURE_TXINV_ENABLE;
hlpuart1.AdvancedInit.RxPinLevelInvert = UART_ADVFEATURE_RXINV_ENABLE;
hlpuart1.FifoMode = UART_FIFOMODE_DISABLE;
if (HAL_UART_Init(&hlpuart1) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_SetTxFifoThreshold(&hlpuart1, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_SetRxFifoThreshold(&hlpuart1, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_DisableFifoMode(&hlpuart1) != HAL_OK)
{
Error_Handler();
}
}In addition, I constantly check error conditions.
bool H747_UART::errorCheck(void)
{
uart_isr_bit.all = uart_handle->Instance->ISR;
if(uart_isr_bit.bits.PE || uart_isr_bit.bits.NE || uart_isr_bit.bits.ORE)
{
return false;
}
return true;
}I could not find the root cause of the problem. I would be glad if you could help.
Sincelery
Solved! Go to Solution.
2021-04-02 2:03 AM
Hi Tesla;
This problem is solved. I overlooked the status of the Frame Error (FE) bit in the ISR error flags. If the serial port line is physically empty, the FE bit is set to 1. I corrected this error situation by setting the FECF bit in the ICR register to 1.
Thanks
2021-04-01 8:12 AM
So what statuses continue to flag?
Show register dump in these situations.
2021-04-02 2:03 AM
Hi Tesla;
This problem is solved. I overlooked the status of the Frame Error (FE) bit in the ISR error flags. If the serial port line is physically empty, the FE bit is set to 1. I corrected this error situation by setting the FECF bit in the ICR register to 1.
Thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.