STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F469I-DISCO FMC WRITE_READ_ADDR 0x0800

HiI just wonder at the example:STM32Cube_FW_F4_V1.26.0/Projects/STM32469I-Discovery/Examples/FMC/FMC_SDRAM/Src/main.cand there is a define:#define WRITE_READ_ADDR ((uint32_t)0x0800)Whats the purpose of that (offset?)? Doesn't the FMC SDRAM start ...

PGroe.2 by Associate III
  • 1067 Views
  • 2 replies
  • 0 kudos

Need help running STM32F4 from internal RAM

Hi Experts,I need to run my code (it is a small code) from internal RAM. It currently runs from the first sector in the flash. For some reason, I need to change a few bytes in the same sector and it seems I can't write to the same sector from where t...

RBharol by Associate III
  • 2888 Views
  • 5 replies
  • 0 kudos

Long Press on flexButton

Hi all,I'm trying to manage a long pression on a Flex button.I want realize this simple algorithm:short pression = action_1()long pression(IE 2secons) = action_2()I enabled clickListener over this Flex button, I configured the trigger event on "Touch...

MPast.1 by Senior II
  • 814 Views
  • 0 replies
  • 0 kudos

I'm having trouble with the STM32F030xC I2C bootloader. I can send a command OK, but get errors from my I2C system (Windows based using FTDI) when I try and read the response. My question relates to an ambiguity in AN4221.

AN4221 says it will enter I2C boot mode on detecting its address and will then start waiting for commands. What is not clear is whether this address is sent as part of the first command, or by some separate undescribed operation. I've tried various a...

Nrose.2 by Associate
  • 752 Views
  • 0 replies
  • 0 kudos

designing at runtime

I want that the user can design the screen at runtime. So I'm trying to add box, text, image to the screen by the user button. I tested font caching for the text and didn't know how to add the text and where it should be. Even the text is cached, ho...

Ezgi by Senior
  • 530 Views
  • 1 replies
  • 0 kudos

STM32 ADC readings are saturating, any thoughts?

So we have just gone into production on a new design, a very small part of the circuit monitors the devices battery voltage fed into one of the ADC channels. I am finding that 1 in every 50 boards has developed a failure with the ADC where it just re...

Rclar.13 by Associate II
  • 6557 Views
  • 12 replies
  • 0 kudos

STM32H750 read USART Rx data via DMA

Dear ST Community,I would like to set up the USART1 and DMA2 in a way, so that the DMA automatically stores the data received by the USART to a buffer variable.To achieve that I used STM32CubeMX to generate the configuration code utilizing the Low Le...

CBrom.1 by Associate II
  • 1422 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.