2023-07-22 5:07 AM - edited 2023-07-22 7:33 AM
Hi guys
After erasing the flash memory with STM32CubeProgrammer, my STM32H745ZI doesn't run CM4 correctly anymore.
I'm experiencing this error:
Break at address "0xfffffffe"
with no debug information available.
Should I need to restore some default configuration after the memory erase?
Thanks ;)
EDIT: Model name updated
2023-07-22 5:20 AM
STM32H743 does not have CM4.
2023-07-22 7:27 AM - edited 2023-07-22 7:30 AM
I'm sorry, there is typo in my previous message.
The board is NUCLEO-H745ZI-Q with STM32H745ZI MCU
2023-07-22 7:53 AM
>>Should I need to restore some default configuration after the memory erase?
Try putting viable code and a vector table in the FLASH, or change option bytes so it's not starting the M4 without anything to run?
2023-07-22 8:39 AM
I have uploaded a working project code to CM4 with Stm32CubeIDE but nothing changed. The board halt before the complete execution of the main() function.
I've also tried to upload a new project with Stm32CubeIDE but there is still this strange error.
I didn't upload nothing to CM7.
2023-07-24 6:00 AM
Something in the option bytes to enable CM4?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.