2023-09-29 8:06 AM
Hello,
I am trying to generate a complementary PWM with a timer in my STM32H723VGTx, I configured channel 1 on timer 1 with the PWM Generation CH1 CH1N mode.
I set all the parameters of the base timer and the value for the pulse of PWM, but during the validation process I didn't have any signal on the CH1N, I even tried on channel 2 but nothing.
Here my functions are then called in main.c:
/* PWM: */
void my_PWM_init(){
// Initialize TIM1 for PWM
TIM_HandleTypeDef htim1;
htim1.Instance = TIM1;
// Start TIM1
HAL_TIM_PWM_Start(&htim1, TIM_CHANNEL_1); // Start channel 1
HAL_TIM_PWM_Start(&htim1, TIM_CHANNEL_2); // Start channel 2 as well
HAL_TIMEx_PWMN_Start(&htim1, TIM_CHANNEL_1);
HAL_TIMEx_PWMN_Start(&htim1, TIM_CHANNEL_2);
// Set PWM parameters for channel 1
Set_PWM_Frequency_DutyCycle(&htim1, 10000, 50, TIM_CHANNEL_1);
// Set PWM parameters for channel 2
Set_PWM_Frequency_DutyCycle(&htim1, 10000, 25, TIM_CHANNEL_2);
}
// Function to set PWM frequency and duty cycle for TIM1 channel
void Set_PWM_Frequency_DutyCycle(TIM_HandleTypeDef *htim, uint32_t frequency_hz, float duty_cycle_percent, uint32_t channel) {
// Calculate the period (ARR) value based on the desired frequency
uint32_t timer_clock = HAL_RCC_GetPCLK2Freq()*2; // Assuming TIM1 is on APB2
uint32_t period = timer_clock / frequency_hz;
// Calculate the pulse (CCR) value based on the desired duty cycle
uint32_t pulse = (uint32_t)(period * (duty_cycle_percent / 100.0f));
// Update TIM1 settings
TIM_OC_InitTypeDef sConfigOC;
sConfigOC.OCMode = TIM_OCMODE_PWM1;
sConfigOC.Pulse = pulse;
sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;
if(HAL_TIM_PWM_ConfigChannel(htim, &sConfigOC, channel) != HAL_OK){
Error_Handler();
}
// Update the period (ARR) value
htim->Instance->ARR = period - 1;
// Set the new pulse (CCR) value
__HAL_TIM_SET_COMPARE(htim, channel, pulse);
}
2023-09-29 8:27 AM
Follow an existing example or refer to the documentation on how to use HAL PWM functions. In particular:
(#) Configure the TIM in the desired functioning mode using one of the
Initialization function of this driver:
(++) HAL_TIM_PWM_Init and HAL_TIM_PWM_ConfigChannel: to use the Timer to generate a
PWM signal.If you're already calling those, show the full code.
> TIM_HandleTypeDef htim1;
> htim1.Instance = TIM1;
You're missing a lot more initialization parameters.
2023-09-29 9:42 AM
Hello @MGian.1
Do you use CubeMX? If yes, please share your IOC file (e.g in excel format ..)
Did you check your hardware configuration in datasheet?
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-10-06 1:12 AM
Hello @FBL,
Here is my entire project!
I am just trying to configure the peripherals for the moment I am testing only.
2023-10-06 5:46 AM
Hello @MGian.1
Make sure that the timer is configured correctly for PWM generation.
This includes setting the correct mode, setting the prescaler and period values, deadtime, and setting the pulse value for the PWM.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-10-06 6:35 AM
Hello @FBL,
The basic setting of the timer is correctly set as the PWM signal on CH1 is correct, the only problem is the complementary signal that is not provided.
I think that I neglected some enable or the pin configuration generated from the .ioc is wrong.
2023-10-06 8:34 AM
Make sure the pin in question works properly (think bad solder joints and shorts), e.g. by setting it as GPIO output and toggling "manually".
If that confirms HW is OK, then read out and check/post content of TIM and relevant GPIO registers.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.