2023-09-06 1:29 AM
Hi,
I am working on freertos plus tcp library with STM32H563ZI, but how must I make memory otions in linker file?
like:
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 320K
FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 2048K
RAM1 (xrw) : ORIGIN = 0x20000000, LENGTH = 256K
RAM2 (xrw) : ORIGIN = 0x20040000, LENGTH = 64K
RAM3 (xrw) : ORIGIN = 0x20050000, LENGTH = 320K
it is wrong I know but how can I make this right ?
2024-04-03 1:04 PM
This is in stm32h5xx_hal_eth.h, use that...
/**
* @brief checks whether the specified ETH WAKEUP Exti interrupt flag is set or not.
* @PAram __EXTI_LINE__: specifies the ETH WAKEUP Exti sources to be cleared.
* @arg ETH_WAKEUP_EXTI_LINE
* @retval EXTI ETH WAKEUP Line Status.
*/
#define __HAL_ETH_WAKEUP_EXTI_GET_FLAG(__EXTI_LINE__) (EXTI->RPR2 & (__EXTI_LINE__))
2024-04-04 12:22 AM
Thank you @Tesla DeLorean for that, I saw what you referred me to, and I can automatically just replace all the relevant different values from the H7 with the H5 ones but I want to use the experience of @Recep that said he have a running project by only replacing the include files and he did not mention changing anything in the files so maybe I'm missing something.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.