2021-04-04 2:15 AM
Hi,
I have a custom board with an STM32G474RE. I use 3 CANs with 3 independent CAN tranciever on the board.
I tried sendind CAN message from CAN1 to CAN3 but the message is not received. At least the callback funnction is not called. I used an oscilloscope to make sure that the message was sent by CAN1 and received on CAN3 pins.
I used the STM CANFD example codes. Unfortunately they use CANFD format and Classical. Maybe that is where I made a mistake.
Any help is much appreciated!
Config and Message sendin in main.c
uint8_t TxData[8] = {0x11,0x22,0x33,0x44,0x55,0x66,0x77,0x88};
FDCAN_Config();
while (1)
{
if (HAL_FDCAN_AddMessageToTxFifoQ(&hfdcan3, &TxHeader, TxData) != HAL_OK)
{
/* Transmission request Error */
Error_Handler();
}
HAL_Delay(10);
}The Callback function in main.c
void HAL_FDCAN_RxFifo0Callback(FDCAN_HandleTypeDef *hfdcan, uint32_t RxFifo0ITs)
{
HAL_GPIO_TogglePin(GPIOC, GPIO_PIN_10);
if((RxFifo0ITs & FDCAN_IT_RX_FIFO0_NEW_MESSAGE) != RESET)
{
/* Retrieve Rx messages from RX FIFO0 */
if (HAL_FDCAN_GetRxMessage(hfdcan, FDCAN_RX_FIFO0, &RxHeader, RxData) != HAL_OK)
{
Error_Handler();
}
/* Display LEDx */
if ((RxHeader.Identifier == 0x201) && (RxHeader.IdType == FDCAN_STANDARD_ID))
{
//HAL_GPIO_TogglePin(GPIOC, GPIO_PIN_10);
}
}
}#include "fdcan.h"
FDCAN_RxHeaderTypeDef RxHeader;
uint8_t RxData[8];
FDCAN_TxHeaderTypeDef TxHeader;
FDCAN_HandleTypeDef hfdcan1;
FDCAN_HandleTypeDef hfdcan2;
FDCAN_HandleTypeDef hfdcan3;
void MX_FDCAN1_Init(void)
{
hfdcan1.Instance = FDCAN1;
hfdcan1.Init.ClockDivider = FDCAN_CLOCK_DIV1;
hfdcan1.Init.FrameFormat = FDCAN_FRAME_CLASSIC;
hfdcan1.Init.Mode = FDCAN_MODE_NORMAL;
hfdcan1.Init.AutoRetransmission = DISABLE;
hfdcan1.Init.TransmitPause = DISABLE;
hfdcan1.Init.ProtocolException = DISABLE;
hfdcan1.Init.NominalPrescaler = 21;
hfdcan1.Init.NominalSyncJumpWidth = 1;
hfdcan1.Init.NominalTimeSeg1 = 5;
hfdcan1.Init.NominalTimeSeg2 = 2;
hfdcan1.Init.DataPrescaler = 21;
hfdcan1.Init.DataSyncJumpWidth = 1;
hfdcan1.Init.DataTimeSeg1 = 5;
hfdcan1.Init.DataTimeSeg2 = 2;
hfdcan1.Init.StdFiltersNbr = 0;
hfdcan1.Init.ExtFiltersNbr = 0;
hfdcan1.Init.TxFifoQueueMode = FDCAN_TX_FIFO_OPERATION;
if (HAL_FDCAN_Init(&hfdcan1) != HAL_OK)
{
Error_Handler();
}
}
void MX_FDCAN2_Init(void)
{
hfdcan2.Instance = FDCAN2;
hfdcan2.Init.FrameFormat = FDCAN_FRAME_CLASSIC;
hfdcan2.Init.Mode = FDCAN_MODE_NORMAL;
hfdcan2.Init.AutoRetransmission = DISABLE;
hfdcan2.Init.TransmitPause = DISABLE;
hfdcan2.Init.ProtocolException = DISABLE;
hfdcan2.Init.NominalPrescaler = 16;
hfdcan2.Init.NominalSyncJumpWidth = 1;
hfdcan2.Init.NominalTimeSeg1 = 25;
hfdcan2.Init.NominalTimeSeg2 = 4;
hfdcan2.Init.DataPrescaler = 1;
hfdcan2.Init.DataSyncJumpWidth = 1;
hfdcan2.Init.DataTimeSeg1 = 25;
hfdcan2.Init.DataTimeSeg2 = 1;
hfdcan2.Init.StdFiltersNbr = 0;
hfdcan2.Init.ExtFiltersNbr = 0;
hfdcan2.Init.TxFifoQueueMode = FDCAN_TX_FIFO_OPERATION;
if (HAL_FDCAN_Init(&hfdcan2) != HAL_OK)
{
Error_Handler();
}
}
/* FDCAN3 init function */
void MX_FDCAN3_Init(void)
{
hfdcan3.Instance = FDCAN3;
hfdcan3.Init.FrameFormat = FDCAN_FRAME_CLASSIC;
hfdcan3.Init.Mode = FDCAN_MODE_NORMAL;
hfdcan3.Init.AutoRetransmission = DISABLE;
hfdcan3.Init.TransmitPause = DISABLE;
hfdcan3.Init.ProtocolException = DISABLE;
hfdcan3.Init.NominalPrescaler = 21;
hfdcan3.Init.NominalSyncJumpWidth = 1;
hfdcan3.Init.NominalTimeSeg1 = 5;
hfdcan3.Init.NominalTimeSeg2 = 2;
hfdcan3.Init.DataPrescaler = 21;
hfdcan3.Init.DataSyncJumpWidth = 1;
hfdcan3.Init.DataTimeSeg1 = 5;
hfdcan3.Init.DataTimeSeg2 = 2;
hfdcan3.Init.StdFiltersNbr = 0;
hfdcan3.Init.ExtFiltersNbr = 0;
hfdcan3.Init.TxFifoQueueMode = FDCAN_TX_FIFO_OPERATION;
if (HAL_FDCAN_Init(&hfdcan3) != HAL_OK)
{
Error_Handler();
}
}
static uint32_t HAL_RCC_FDCAN_CLK_ENABLED=0;
void HAL_FDCAN_MspInit(FDCAN_HandleTypeDef* fdcanHandle)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
if(fdcanHandle->Instance==FDCAN1)
{
HAL_RCC_FDCAN_CLK_ENABLED++;
if(HAL_RCC_FDCAN_CLK_ENABLED==1){
__HAL_RCC_FDCAN_CLK_ENABLE();
}
__HAL_RCC_GPIOA_CLK_ENABLE();
GPIO_InitStruct.Pin = MSCAN_RX_Pin|MSCAN_TX_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.Alternate = GPIO_AF9_FDCAN1;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/* FDCAN1 interrupt Init */
HAL_NVIC_SetPriority(FDCAN1_IT0_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(FDCAN1_IT0_IRQn);
HAL_NVIC_SetPriority(FDCAN1_IT1_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(FDCAN1_IT1_IRQn);
}
else if(fdcanHandle->Instance==FDCAN2)
{
HAL_RCC_FDCAN_CLK_ENABLED++;
if(HAL_RCC_FDCAN_CLK_ENABLED==1){
__HAL_RCC_FDCAN_CLK_ENABLE();
}
__HAL_RCC_GPIOB_CLK_ENABLE();
GPIO_InitStruct.Pin = SWCAN_RX_3V3_Pin|SWCAN_RX_3V3B6_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.Alternate = GPIO_AF9_FDCAN2;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
/* FDCAN2 interrupt Init */
HAL_NVIC_SetPriority(FDCAN2_IT0_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(FDCAN2_IT0_IRQn);
HAL_NVIC_SetPriority(FDCAN2_IT1_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(FDCAN2_IT1_IRQn);
}
else if(fdcanHandle->Instance==FDCAN3)
{
HAL_RCC_FDCAN_CLK_ENABLED++;
if(HAL_RCC_FDCAN_CLK_ENABLED==1){
__HAL_RCC_FDCAN_CLK_ENABLE();
}
__HAL_RCC_GPIOA_CLK_ENABLE();
GPIO_InitStruct.Pin = HSCAN_RX_Pin|HSCAN_TX_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.Alternate = GPIO_AF11_FDCAN3;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/* FDCAN3 interrupt Init */
HAL_NVIC_SetPriority(FDCAN3_IT0_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(FDCAN3_IT0_IRQn);
HAL_NVIC_SetPriority(FDCAN3_IT1_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(FDCAN3_IT1_IRQn);
}
}
void HAL_FDCAN_MspDeInit(FDCAN_HandleTypeDef* fdcanHandle)
{
if(fdcanHandle->Instance==FDCAN1)
{
HAL_RCC_FDCAN_CLK_ENABLED--;
if(HAL_RCC_FDCAN_CLK_ENABLED==0){
__HAL_RCC_FDCAN_CLK_DISABLE();
}
HAL_GPIO_DeInit(GPIOA, MSCAN_RX_Pin|MSCAN_TX_Pin);
/* FDCAN1 interrupt Deinit */
HAL_NVIC_DisableIRQ(FDCAN1_IT0_IRQn);
HAL_NVIC_DisableIRQ(FDCAN1_IT1_IRQn);
}
else if(fdcanHandle->Instance==FDCAN2)
{
HAL_RCC_FDCAN_CLK_ENABLED--;
if(HAL_RCC_FDCAN_CLK_ENABLED==0){
__HAL_RCC_FDCAN_CLK_DISABLE();
}
HAL_GPIO_DeInit(GPIOB, SWCAN_RX_3V3_Pin|SWCAN_RX_3V3B6_Pin);
/* FDCAN2 interrupt Deinit */
HAL_NVIC_DisableIRQ(FDCAN2_IT0_IRQn);
HAL_NVIC_DisableIRQ(FDCAN2_IT1_IRQn);
}
else if(fdcanHandle->Instance==FDCAN3)
{
HAL_RCC_FDCAN_CLK_ENABLED--;
if(HAL_RCC_FDCAN_CLK_ENABLED==0){
__HAL_RCC_FDCAN_CLK_DISABLE();
}
HAL_GPIO_DeInit(GPIOA, HSCAN_RX_Pin|HSCAN_TX_Pin);
/* FDCAN3 interrupt Deinit */
HAL_NVIC_DisableIRQ(FDCAN3_IT0_IRQn);
HAL_NVIC_DisableIRQ(FDCAN3_IT1_IRQn);
}
}
/* USER CODE BEGIN 1 */
void FDCAN_Config(void)
{
FDCAN_FilterTypeDef sFilterConfig;
/* Configure Rx filter */
sFilterConfig.IdType = FDCAN_STANDARD_ID;
sFilterConfig.FilterIndex = 0;
sFilterConfig.FilterType = FDCAN_FILTER_MASK;
sFilterConfig.FilterConfig = FDCAN_FILTER_TO_RXFIFO0;
sFilterConfig.FilterID1 = 0x201;
if (HAL_FDCAN_ConfigFilter(&hfdcan1, &sFilterConfig) != HAL_OK)
{
Error_Handler();
}
if (HAL_FDCAN_ConfigFilter(&hfdcan3, &sFilterConfig) != HAL_OK)
{
Error_Handler();
}
if (HAL_FDCAN_ConfigGlobalFilter(&hfdcan1, FDCAN_REJECT, FDCAN_REJECT, FDCAN_FILTER_REMOTE, FDCAN_FILTER_REMOTE) != HAL_OK)
{
Error_Handler();
}
if (HAL_FDCAN_ConfigGlobalFilter(&hfdcan3, FDCAN_REJECT, FDCAN_REJECT, FDCAN_FILTER_REMOTE, FDCAN_FILTER_REMOTE) != HAL_OK)
{
Error_Handler();
}
/* Start the FDCAN module */
if (HAL_FDCAN_Start(&hfdcan1) != HAL_OK)
{
Error_Handler();
}
if (HAL_FDCAN_Start(&hfdcan3) != HAL_OK)
{
Error_Handler();
}
if (HAL_FDCAN_ActivateNotification(&hfdcan1, FDCAN_IT_RX_FIFO0_NEW_MESSAGE, 0) != HAL_OK)
{
Error_Handler();
}
if (HAL_FDCAN_ActivateNotification(&hfdcan3, FDCAN_IT_RX_FIFO0_NEW_MESSAGE, 0) != HAL_OK)
{
Error_Handler();
}
/* Prepare Tx Header */
TxHeader.Identifier = 0x201;
TxHeader.IdType = FDCAN_STANDARD_ID;
TxHeader.TxFrameType = FDCAN_FRAME_CLASSIC;
TxHeader.DataLength = FDCAN_DLC_BYTES_8;
TxHeader.ErrorStateIndicator = FDCAN_ESI_ACTIVE;
TxHeader.BitRateSwitch = FDCAN_BRS_OFF;
TxHeader.FDFormat = FDCAN_CLASSIC_CAN;
TxHeader.TxEventFifoControl = FDCAN_NO_TX_EVENTS;
TxHeader.MessageMarker = 0;
}
CAN Config file
2021-04-04 2:32 AM
Something wrong with the filtering. I am not sure what.
Commeting that section makes it work. Without filtering of course.
I can't find any good description for classic frame with FDCAN MCUs.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.