2025-01-18 2:53 AM - edited 2025-01-18 2:54 AM
Hello,
I'am currently programming on a STM32G473. I'am sending CAN Message via the FDCAN peripheral.
In generally everything works, all my messages I put into the Tx Buffer are sent.
But in one little detail I'am confused:
In Figure 669 its described, that the TX buffer consists of 3 elements.
But if I want to find out in which index I have to put the next message by reading the TXFQS_TFQPI field, I'am confused why the reference manual describes a range of 0-3 for this field. So it seems that there are 4 messages? But in the Add-Request Register (TXBAR_AR) there are only 3 Bits for adding transmission requests (and the RAM buffer has only space for 3 Messages).
So is it maybe an error in the reference manual and the range of TXFQS_TFQPI is only 0-2 and in reality the peripheral will never give me a 3 in this field?
Or, if the range 0-3 is correct: What should I do if I get a put-Index of 3?
[Ref: RM0440, Rev. 8]
2025-01-18 7:36 AM
Good catch!
I think You are right this is a error in the Reference manual.
At least the HAL driver uses the TFQPI field with out any check for values > 2 (this would write the Message outside of the Message RAM!).
Let's see if some one from ST has some insight.
Martin
2025-01-18 12:34 PM
Perhaps 3 means the buffer is full.
And there is nowhere else to write))
2025-01-19 9:34 AM
If this were the case then the HAL driver would lose TX messages (writing outside the Buffer memory and enabling a not present TXBAR AR Bit!)
2025-01-19 10:56 PM - edited 2025-01-19 10:57 PM
@Oleksii: I dont think so. There is a dedicated Bit TXFQS_TFQF which is the "Tx FIFO/Queue full" indication.
2025-01-20 12:03 AM
Have you ever thought about the fact that 3 (0b11),
is a trigger for the bit TXFQS_TFQF = 1))
2025-01-20 12:07 AM
HAL_StatusTypeDef HAL_FDCAN_AddMessageToTxFifoQ(FDCAN_HandleTypeDef *hfdcan, const FDCAN_TxHeaderTypeDef *pTxHeader,
const uint8_t *pTxData)
{
uint32_t PutIndex;
/* Check function parameters */
assert_param(IS_FDCAN_ID_TYPE(pTxHeader->IdType));
if (pTxHeader->IdType == FDCAN_STANDARD_ID)
{
assert_param(IS_FDCAN_MAX_VALUE(pTxHeader->Identifier, 0x7FFU));
}
else /* pTxHeader->IdType == FDCAN_EXTENDED_ID */
{
assert_param(IS_FDCAN_MAX_VALUE(pTxHeader->Identifier, 0x1FFFFFFFU));
}
assert_param(IS_FDCAN_FRAME_TYPE(pTxHeader->TxFrameType));
assert_param(IS_FDCAN_DLC(pTxHeader->DataLength));
assert_param(IS_FDCAN_ESI(pTxHeader->ErrorStateIndicator));
assert_param(IS_FDCAN_BRS(pTxHeader->BitRateSwitch));
assert_param(IS_FDCAN_FDF(pTxHeader->FDFormat));
assert_param(IS_FDCAN_EFC(pTxHeader->TxEventFifoControl));
assert_param(IS_FDCAN_MAX_VALUE(pTxHeader->MessageMarker, 0xFFU));
if (hfdcan->State == HAL_FDCAN_STATE_BUSY)
{
/* Check that the Tx FIFO/Queue is not full */
if ((hfdcan->Instance->TXFQS & FDCAN_TXFQS_TFQF) != 0U)
{
/* Update error code */
hfdcan->ErrorCode |= HAL_FDCAN_ERROR_FIFO_FULL;
return HAL_ERROR;
}
else
{
/* Retrieve the Tx FIFO PutIndex */
PutIndex = ((hfdcan->Instance->TXFQS & FDCAN_TXFQS_TFQPI) >> FDCAN_TXFQS_TFQPI_Pos);
/* Add the message to the Tx FIFO/Queue */
FDCAN_CopyMessageToRAM(hfdcan, pTxHeader, pTxData, PutIndex);
/* Activate the corresponding transmission request */
hfdcan->Instance->TXBAR = ((uint32_t)1 << PutIndex);
/* Store the Latest Tx FIFO/Queue Request Buffer Index */
hfdcan->LatestTxFifoQRequest = ((uint32_t)1 << PutIndex);
}
/* Return function status */
return HAL_OK;
}
else
{
/* Update error code */
hfdcan->ErrorCode |= HAL_FDCAN_ERROR_NOT_STARTED;
return HAL_ERROR;
}
}Automatic platoon TXFQS_TFQF = 1,
Does not lead to message loss.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.