2017-01-12 10:25 AM
I should not have to edit a conf file to build an example specific to the hardware, but ok
bug #1
Building file: /Users/john/STM32Cube/Repository/STM32Cube_FW_F7_V1.5.1/Utilities/Log/lcd_log.c Invoking: MCU GCC Compiler /Users/john/STM32Cube/Repository/STM32Cube_FW_F7_V1.5.1/Projects/STM32F769I-Discovery/Examples/BSP/SW4STM32/STM32769I-Discovery/Debug arm-none-eabi-gcc -mthumb -mfloat-abi=soft -O0 -g3 -Wall -fmessage-length=0 -ffunction-sections -c -MMD -MP -MF'Utilities/lcd_log.d' -MT'Utilities/lcd_log.o' -o 'Utilities/lcd_log.o' '/Users/john/STM32Cube/Repository/STM32Cube_FW_F7_V1.5.1/Utilities/Log/lcd_log.c' In file included from /Users/john/STM32Cube/Repository/STM32Cube_FW_F7_V1.5.1/Utilities/Log/lcd_log.c:51:0: /Users/john/STM32Cube/Repository/STM32Cube_FW_F7_V1.5.1/Utilities/Log/lcd_log.h:44:26: fatal error: lcd_log_conf.h: No such file or directory #include 'lcd_log_conf.h' ^ compilation terminated. make: *** [Utilities/lcd_log.o] Error 1 12:17:47 Build Finished (took 2s.37ms)
so, ok, I edit the conf file and change
#include 'stm32xxx_eval_lcd.h' /* replace 'stm32xxx' with your EVAL board name, ex: stm324x9i_eval_lcd.h */
to
#include 'stm32f769i_discovery_lcd.h'
which yields bug #2:
Building file: /Users/john/STM32Cube/Repository/STM32Cube_FW_F7_V1.5.1/Utilities/Log/lcd_log.c
Invoking: MCU GCC Compiler/Users/john/STM32Cube/Repository/STM32Cube_FW_F7_V1.5.1/Projects/STM32F769I-Discovery/Examples/BSP/SW4STM32/STM32769I-Discovery/Debugarm-none-eabi-gcc -mthumb -mfloat-abi=soft -O0 -g3 -Wall -fmessage-length=0 -ffunction-sections -c -MMD -MP -MF'Utilities/lcd_log.d' -MT'Utilities/lcd_log.o' -o 'Utilities/lcd_log.o' '/Users/john/STM32Cube/Repository/STM32Cube_FW_F7_V1.5.1/Utilities/Log/lcd_log.c'In file included from /Users/john/STM32Cube/Repository/STM32Cube_FW_F7_V1.5.1/Utilities/Log/lcd_log.h:44:0, from /Users/john/STM32Cube/Repository/STM32Cube_FW_F7_V1.5.1/Utilities/Log/lcd_log.c:51:/Users/john/STM32Cube/Repository/STM32Cube_FW_F7_V1.5.1/Utilities/Log/lcd_log_conf.h:51:39: fatal error: stm32f769i_discovery_lcd.h: No such file or directory #include 'stm32f769i_discovery_lcd.h' ^compilation terminated.make: *** [Utilities/lcd_log.o] Error 112:23:24 Build Finished (took 1s.252ms)
2017-01-12 1:49 PM
Looks like you need to add to the Include Paths
2017-01-12 6:16 PM
Thank you Clive One, you're awesome.
Indeed, FW_F7_1.5.0 has very different include paths from FW_F7_1.5.1.
when i check the properties (sw4stm32) it shows no include paths for GNU C and they're all in Assembly in version 1.5.1.
In 1.5.0, they're fine in GNU C but no paths shown in Assembly section of the Paths & Symbols part of the properties
FW_F7_1.5.0 builds and runs right out of the box with no hand-waving required
Thanks again. This is so much more fun, an easier to learn from, when the examples work as advertised.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.