2017-01-12 7:35 AM
Hello!
I have a question about STM32F429-Disco evaluation board. As I see, LD3985 is used to supply the power to all on-board units (MCU, LCD, MEMS, SDRAM and others). But as it is written in LD3985 datasheet, it can provide only 150 mA output current. I think it's not enough for all these modules... How does this board work? =)
Thank you in advance!
#schematic #ld3985 #stm32f429-disco #evaluation-boards #power-supplySolved! Go to Solution.
2017-01-12 8:47 AM
Good question, the specification seems to suggest it can get north of 550mA and remain within 5% of regulation, but to be honest I've not checked on what the nominal loading is for all the components on the board, including the back-light.
http://www.mouser.com/ds/2/389/CD00003395-470441.pdf
2017-01-12 8:47 AM
Good question, the specification seems to suggest it can get north of 550mA and remain within 5% of regulation, but to be honest I've not checked on what the nominal loading is for all the components on the board, including the back-light.
http://www.mouser.com/ds/2/389/CD00003395-470441.pdf
2017-01-12 11:30 AM
550 mA should be enough I think... But is it safely to use LD3985 in this mode for a long time (when it operates with peak current)?
2017-01-12 12:17 PM
I haven't analyzed the design, I doubt it is anywhere near 550mA, closer to 200mA I expect.
2017-01-12 1:14 PM
Ok, thank you!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.