2016-11-20 5:50 AM
Hi,
I'am trying to get the audio from WM8994 line input.The BSP driver seems rather incomplete, it works with the 4 mems mics but not with the line input from the codec.Is there somewhere any source code example for that ? anyone facing the same problem ?I can share some code that tries to do playback from line in to headphone out if someone interested.RegardsFrancois #stm32f769i-disco-audio-wm89942017-04-04 6:36 PM
when you say 'noisy' do you mean line noise? like static or something?
2017-05-27 7:21 AM
It actually sounds nice if you back off on the input signal strength. it is after all, line level in not speaker in.
2017-05-28 2:33 PM
Thank you
Beaulier.Francois
2018-03-25 12:36 AM
thanks a lot for posting this code john. did you run into issues with noise on the codec's line in? I get enough noise to make the board unusable for audio processing with the code you posted, and with ST's audio loopback demo (which may be new.) I tried powering the board from an external linear Psu as well. gonna have a look at the hefty datasheet of the WM8994 to see if I can reduce the noise by changing some analog path settings or something.
2019-02-12 8:49 AM
I had a similar problem on my STM32F723E-disco board. Noise level on line-in input was unacceptable. Problem lied in wrong connection between PC and board. Supplying power from phone charger solved this issue. More can be found here: https://forum.cockos.com/showthread.php?t=113721
2020-01-30 8:28 PM
its very great example... thank.. but i want 8K audio frequency & it not working... it working just >= 16K audio frequency... can u tell me why? because i want slow speed DSP audio
2020-12-05 3:58 AM
I am also facing same problem to get analog audio signal from line in jack at stm32f769i discovery board.
If you have this code,Please share whole working zipped project file.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.