2016-03-25 6:39 AM
Hello! I want to connect tft display with 1280*720 resolution via DSI interface. TFT panel has 4 differential inputs for data. There is no reference manual for stm32f769 controller on this page http://www.st.com/web/en/catalog/mmc/FM141/SC1169/SS1858/LN1999, so i don't know, what is the maximum resolution for DSI interface. Can i use such lcd with stm32f769 controller? Thank you.
2016-03-25 7:07 AM
Hi dmitriev.artyomNo,
As it is mentioned in the STM32F769xx related data brief the MIPI® DSI host controller supports up to 720p 30 Hz resolution.If you need more information please contact your FAE or local representative.-Syrine-2016-03-28 11:24 PM
So it is not possible to control lcds with more than 2 data lines? Is it right?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.