2019-06-14 12:19 PM
Dear support,
We use 3 cans in STM32F767ZI board and have some problems with filter & banks configurations.
We use FilterScale = CAN_FILTERSCALE_32BIT and CAN_ID_EXT for transmit/receive data. We would like to receive data by the following way: CAN1 should receive all data with bits[9-12]=0001, CAN2 should receive all data with bits[9-12]=0002, CAN3 should receive all data with bits[9-12]=0003.
we set:
filter_id1 = 0x00000200;
filter_id2 = 0x00000400 ;
filter_id3 = 0x00000600;
filter_mask1 = 0x00000200;
filter_mask2 = 0x00000400;
filter_mask3 = 0x00000600;
but these setting don't work properly. Could you pls help to understand what it is a problem here.
And another question about banks. we use :
can1: sFilterConfigCan1.FilterBank = 0, sFilterConfigCan1.SlaveStartFilterBank = 14;
can2: sFilterConfigCan1.FilterBank = 14, sFilterConfigCan1.SlaveStartFilterBank = 14;
can3: sFilterConfigCan1.FilterBank = 2, sFilterConfigCan1.SlaveStartFilterBank = 14;
Is it correct setting?
Thanks, Sabina
Solved! Go to Solution.
2019-06-16 4:05 AM
The problem is resolved.
Now all 3 cans work with filters. if somebody need it the configuration for 3 Cans with EXT ID should be:
can1: FIFO0; sFilterConfigCan1.FilterBank = 0, sFilterConfigCan1.SlaveStartFilterBank = 0;
can2: FIFO1; sFilterConfigCan1.FilterBank = 4, sFilterConfigCan1.SlaveStartFilterBank = 4;
can3: sFilterConfigCan1.FilterBank = 11, sFilterConfigCan1.SlaveStartFilterBank = 11;
We had to choose banks that support ID List (32-bits) .
About Filters:
Uint32 filter_id1 = 0x00000200;//will catch all with IDs 1
Uint32 filter_id2 = 0x00000400 ;//will catch all with IDs 2
Uint32 filter_id3 = 0x00000600;////will catch all with IDs 3
Uint32 filter_mask1 = 0x00000F00;
Uint32 filter_mask2 = 0x00000F00;
Uint32 filter_mask3 = 0x00000F00;
sFilterConfig.FilterIdLow = (uint16_t) (id << 3);
sFilterConfig.FilterIdLow |= CAN_ID_EXT;
sFilterConfig.FilterIdHigh = (uint16_t) (id >> 13);
sFilterConfig.FilterMaskIdLow =(uint16_t) (mask << 3);
sFilterConfig.FilterMaskIdLow |= CAN_ID_EXT;
sFilterConfig.FilterMaskIdHigh = (uint16_t)(mask >> 13);
Thanks,Sabina
2019-06-16 4:05 AM
The problem is resolved.
Now all 3 cans work with filters. if somebody need it the configuration for 3 Cans with EXT ID should be:
can1: FIFO0; sFilterConfigCan1.FilterBank = 0, sFilterConfigCan1.SlaveStartFilterBank = 0;
can2: FIFO1; sFilterConfigCan1.FilterBank = 4, sFilterConfigCan1.SlaveStartFilterBank = 4;
can3: sFilterConfigCan1.FilterBank = 11, sFilterConfigCan1.SlaveStartFilterBank = 11;
We had to choose banks that support ID List (32-bits) .
About Filters:
Uint32 filter_id1 = 0x00000200;//will catch all with IDs 1
Uint32 filter_id2 = 0x00000400 ;//will catch all with IDs 2
Uint32 filter_id3 = 0x00000600;////will catch all with IDs 3
Uint32 filter_mask1 = 0x00000F00;
Uint32 filter_mask2 = 0x00000F00;
Uint32 filter_mask3 = 0x00000F00;
sFilterConfig.FilterIdLow = (uint16_t) (id << 3);
sFilterConfig.FilterIdLow |= CAN_ID_EXT;
sFilterConfig.FilterIdHigh = (uint16_t) (id >> 13);
sFilterConfig.FilterMaskIdLow =(uint16_t) (mask << 3);
sFilterConfig.FilterMaskIdLow |= CAN_ID_EXT;
sFilterConfig.FilterMaskIdHigh = (uint16_t)(mask >> 13);
Thanks,Sabina
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.