STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Flash loader demonstrator issue

Hi everyone,I have some issue with the Flash loader demonstrator V2.8.0. It has worked several times before. Now when I started the tool, the first step picture 1 (connect to devise) it works fine. But the in the second step picture 2, I can't see an...

An Ha by Associate II
  • 3082 Views
  • 2 replies
  • 0 kudos

ST Motor Control Workbench Error

STM32CubeMX:5.2.1Target Toolchain: ST STM32CubeIDEFirmware Package: V1.10Drive Tye: HALMC Frmware Library: 5.4.0 After I format my computer, I reinstalled Motor Control Workbench.Code generation has a error "Can't add MW MotorControl"My OS use Korean...

MYu by Associate II
  • 831 Views
  • 0 replies
  • 0 kudos

Rotary Encoder using STM32F103C8T6

I am using STM32F103C8T6 MCU. I have Rotary Encoder having 5000 Pulse Per Revolution.I want to count Encoder Pulses and uses only one output from encoder channel A.I also want interrupt after particular number of pulses for example after 17000 pulses...

JPanc.1 by Associate II
  • 2246 Views
  • 3 replies
  • 0 kudos

IDD measurement in STM32L4R9AI

I am trying to measure the IDD on the STM32L4R9AI-EVAL board by connecting a hand-held meter to the jumper JP4 in different low power modes. I am seeing a current of about 220 uA in all of the three stop modes (0, 1 and 2). This seems to be higher th...

KV by Associate
  • 1179 Views
  • 1 replies
  • 0 kudos

STM32F469I-DISCO CAN2 not working

I'm trying to use CAN2 on STM32F469I-DISCO board. I connected SN65HVD232 to CN12 connector 9 (PB5 RX) and 10 (PB13 TX). On pin 9 i can see with Saleae proper CAN data frame with baud 125000. But uC doesn't receive any frame and not generating IT.I tr...

zenobik by Associate II
  • 1413 Views
  • 2 replies
  • 0 kudos

Resolved! Issue with STM32F4 CAN Bus Clock Settings

Hi, Following is my init code for stm32f4 CAN Bus Normal mode. I've Calculated the bus to work on bit rate of 500 kbps & 16 Tq's. If i connect two discovery boards with transceivers(TJA1050) on both sides, i can see CAN data getting transmit...

LRPS_92 by Associate II
  • 3484 Views
  • 4 replies
  • 0 kudos

Resolved! Is i t possible peripheral bit-band in STM32F3 series?

Hi.I'm using a stm32f301k8u but the peripheral bit-band doesn't work.SRAM bit-band work, but peripheral bit-band doesn't work.The previously used STM32F1 and STM32F4 worked well.Is i t possible peripheral bit-band in STM32F3 series?I can't find anyth...

Nnam.12 by Associate
  • 1103 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.