2020-04-18 4:12 AM
Hi.
I am trying to read 4 ADC Channels sequentially in interrupt mode: ADC2_IN7, ADC2_IN14, ADC2_IN15 and ADC2_IN8. However it only reads the last rank channel every time. Please help me understand what I'm doing wrong.
Compiler: IAR Workbench v8.32.1
MCU: STM32F767II
Hardware: Custom PCB
HAL Version: V1.15.0
void main (void)
{
...
Analogue_Inputs_Initialise();
...
while(1)
{
ADC_CH_Rank_ctr = 1;
HAL_ADC_Start_IT(&ADC3Handle);
HAL_Delay(100);
}
}
void Analogue_Inputs_Initialise (void)
{
GPIO_InitTypeDef GPIO_InitStruct;
ADC_ChannelConfTypeDef sConfig;
/********************************
* ADC 3 - AI1, AI2, AI3, AI4 *
********************************/
// Configure ADC Clock
__HAL_RCC_ADC3_CLK_ENABLE();
// Analogue Input 1 - PF7 - ADC3_IN5
// Analogue Input 2 - PF8 - ADC3_IN6
__HAL_RCC_GPIOF_CLK_ENABLE();
GPIO_InitStruct.Pin = GPIO_PIN_7 | GPIO_PIN_8;
GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOF, &GPIO_InitStruct);
// Analogue Input 3 - PC1 - ADC3_IN11
__HAL_RCC_GPIOC_CLK_ENABLE();
GPIO_InitStruct.Pin = GPIO_PIN_1;
GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
// Analogue Input 4 - PA0 - ADC3_IN0
__HAL_RCC_GPIOA_CLK_ENABLE();
GPIO_InitStruct.Pin = GPIO_PIN_0;
GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
// Configure the ADC3 peripheral
ADC3Handle.Instance = ADC3;
ADC3Handle.Init.ClockPrescaler = ADC_CLOCKPRESCALER_PCLK_DIV8;
ADC3Handle.Init.Resolution = ADC_RESOLUTION_12B;
ADC3Handle.Init.ScanConvMode = ENABLE;
ADC3Handle.Init.ContinuousConvMode = ENABLE;
ADC3Handle.Init.DiscontinuousConvMode = DISABLE;
ADC3Handle.Init.NbrOfDiscConversion = 0;
ADC3Handle.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
ADC3Handle.Init.ExternalTrigConv = ADC_SOFTWARE_START;
ADC3Handle.Init.DataAlign = ADC_DATAALIGN_RIGHT;
ADC3Handle.Init.NbrOfConversion = 4;
ADC3Handle.Init.DMAContinuousRequests = DISABLE;
ADC3Handle.Init.EOCSelection = ADC_EOC_SEQ_CONV;
HAL_ADC_Init(&ADC3Handle);
// Analogue Input 1 - PF7 - ADC3_IN5
sConfig.Channel = ADC_CHANNEL_5;
sConfig.Rank = ADC_REGULAR_RANK_1;
sConfig.SamplingTime = ADC_SAMPLETIME_480CYCLES;
sConfig.Offset = 0;
HAL_ADC_ConfigChannel(&ADC3Handle, &sConfig);
// Analogue Input 2 - PF8 - ADC3_IN6
sConfig.Channel = ADC_CHANNEL_6;
sConfig.Rank = ADC_REGULAR_RANK_2;
sConfig.SamplingTime = ADC_SAMPLETIME_480CYCLES;
sConfig.Offset = 0;
HAL_ADC_ConfigChannel(&ADC3Handle, &sConfig);
// Analogue Input 3 - PC1 - ADC3_IN11
sConfig.Channel = ADC_CHANNEL_11;
sConfig.Rank = ADC_REGULAR_RANK_3;
sConfig.SamplingTime = ADC_SAMPLETIME_480CYCLES;
sConfig.Offset = 0;
HAL_ADC_ConfigChannel(&ADC3Handle, &sConfig);
// Analogue Input 4 - PA0 - ADC3_IN0
sConfig.Channel = ADC_CHANNEL_0;
sConfig.Rank = ADC_REGULAR_RANK_4;
sConfig.SamplingTime = ADC_SAMPLETIME_480CYCLES;
sConfig.Offset = 0;
HAL_ADC_ConfigChannel(&ADC3Handle, &sConfig);
// NVIC configuration for ADC Reception complete interrupt
HAL_NVIC_SetPriority(ADC_IRQn, 6, 0);
HAL_NVIC_EnableIRQ(ADC_IRQn);
}
void ADC_IRQHandler(void)
{
HAL_ADC_IRQHandler(&ADC3Handle);
}
void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef* AdcHandle)
{
if( __HAL_ADC_GET_FLAG( AdcHandle, ADC_FLAG_EOC ) )
{
switch( ADC_CH_Rank_ctr )
{
case 1: HMI_Inputs_Outputs.Analog_Input_CH_1 = HAL_ADC_GetValue(AdcHandle); ADC_CH_Rank_ctr++; break;
case 2: HMI_Inputs_Outputs.Analog_Input_CH_2 = HAL_ADC_GetValue(AdcHandle); ADC_CH_Rank_ctr++; break;
case 3: HMI_Inputs_Outputs.Analog_Input_CH_3 = HAL_ADC_GetValue(AdcHandle); ADC_CH_Rank_ctr++; break;
case 4: HMI_Inputs_Outputs.Analog_Input_CH_4 = HAL_ADC_GetValue(AdcHandle);
ADC_CH_Rank_ctr++;
HAL_ADC_Stop_IT(&ADC3Handle);
break;
default: /* Do Nothing */ break;
}
}
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.