2015-11-30 4:53 AM
hello
I make custom board with sdram and use stm32f756 chip. Then I try to run modyfied my self version of uclinux (and u-boot) - but system hangs. this is callstack that I build with 2 leds (early printk don't work) /fs/super.c -> get_sb_single(...) hangs on -> simple_set_mnt(mnt, s); /fs/namespace.c -> void simple_set_mnt(struct vfsmount *mnt, struct super_block *sb) hangs on -> mnt->mnt_root = dget(sb->s_root); /include/linux/dcache.h -> static inline struct dentry *dget(struct dentry *dentry) hangs on -> atomic_inc(&dentry->d_count); /arch/arm/include/asm/atomic.h => atomic_inc( hangs on - atomic_add( Run hangs in this asm code: static inline void atomic_add(int i, atomic_t *v) { unsigned long tmp; int result; //stm32f7_gpio_led_on(1,1); __asm__ __volatile__(''@ atomic_add\n'' ''1: ldrex %0, [%2]\n'' '' add %0, %0, %3\n'' '' strex %1, %0, [%2]\n'' '' teq %1, &sharp0\n'' '' bne 1b'' : ''=&r'' (result), ''=&r'' (tmp) : ''r'' (&v->counter), ''Ir'' (i) : ''cc''); //stm32f7_gpio_led_on(1,0); //stm32f7_gpio_led_on(0,1); } this function is call many times but in this order fail (hangs always on this place). I run ram test in u-boot - but all is ok. Does anyone have a similar problem or know what's up? #uclinux2015-11-30 6:20 AM
I might add
- board is 4 layer (2 layer supply) -sdram tracks are max 12cm - length matched, differences are max 2,5cm. EDIT. Wrong tracks length matching. Kernel loaded to other address run different.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.