2018-07-23 9:37 PM
I broke the USB connector on my disco board so can't flash it. Does anyone have experience using an external ST-Link debugger via the CN8 connector?
2018-08-10 4:49 AM
STM32746G-DISCO?
CN8 is going to be entirely useless, it is there to program the STM32F103 of the ST-LINK
Where you need to get connectivity is the target side of SB14, SB15, SB16 and SB17, and removing the 0-ohm resistors.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.