2018-01-10 12:56 PM
Hello,
I've just built the UART sample code for the 722ze Nucleo board and have a problem. I have not modified the code (except for the transmitted character buffer). The sample code shows setting up the unit for a 9600 N81 format. The character buffer that is transmitted is 153 characters long. When I transmit from the Nucleo I receive the correct number of characters on the RealTerm serial capture program but it's gibberish. None of the ASCII characters are discernable and I can't make heads or tails of how the bits might be shifted... For example, I am sending '12345' which in hex is 0x31 0x32 0x33 0x34 0x35 and I receive 0xEB 0x9B 0x99 0x97 0x95.
Has anyone seen anything like this?
2018-12-12 10:15 AM
>>I understand
Not sure you do, you seem confused.
The NUCLEO-H743ZI has a USART connected to the VCP provide by the ST-LINK, you can send data to the USART on the H7 side and get the data on a PC side terminal application.
You can also connect a SiLabs CP2102 type USB-to-CMOS Serial dongle to any of the other available USART on the board.
You can also use the Serial Wire Viewer (SWV SWO/PB3) as a debug terminal.
2018-12-12 10:54 AM
Hi Clive,
You right. I just got a board today, so I am a bit too much enthusiastic..
I managed to see printf using the SWV.
But I don't understand the 1st option you've mentioned:
"The NUCLEO-H743ZI has a USART connected to the VCP provide by the ST-LINK"
How do I use this UART, which UART number is it ? Is there an example showing how to use it (actually I tried all examples).
Thanks!
ran
2018-12-12 11:36 AM
The User Manual and Schematic indicate it is USART3 on PD8/PD9
2018-12-12 1:37 PM
Right, I wonder why there was no example using this USART3...
I shall try it. Thanks !
2018-12-13 7:07 AM
It does work with USART3, just what I needed ! Thanks a lot
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.