2016-04-12 8:44 AM
In my understanding, DTCM, SRAM1 and SRAM2 all offer single cycle access. This leads my to the conclusion, that enabling DCACHE in a situation where there is no slow external memory does not bring any advantage, but the disadvantage of possible cache incoherencies. Is my understanding right?
Thanks #cache #performance #stm32f7 #dcache2016-04-12 10:41 AM
One reason to enable DCACHE is to cahce access to constant data in flash. But still please comment on my reasoning about DCACHE for SRMA1/SRAM2 access. DTCM is not cached at all in my understanding.
2016-04-12 11:01 AM
Hi bonnes.uwe,
DCACHE can be enabled to cache access for all memories related to AXI bus ( not the case for ITCM and DTCM which have 64-bit access). There is no relation between cache enabling and Slow/fast or external/ internal memroies -> Cache always enhance performance in all cases. To prevent incoherence that may happen, you should make write-through operation. For more details about STM32F7 performance, plesase refere to the application note '' STM32F7 series system architecture and performance'', and you can test the firmware example done with QSPI :http://www.st.com/web/catalog/tools/FM147/CL1794/SC961/SS1743/LN1920/PF262415
-Hannibal-We’re moving the ST Community to a new platform to give you a better and more reliable community experience.