2015-10-12 7:03 AM
I wanted to make a blinky example (LD1) on my STM32F7 DIscovery using HAL drivers as HAL_GPIO_WritePin(GPIOI, GPIO_PIN_1,GPIO_PIN_SET); with no result, then i resolve that i could use BSP drivers, but i had this error: Error &sharp545: Required gpdsc file 'C:\Users\Lenovo Y560\STM32Cube\Repository\STM32Cube_FW_F7_V1.1.0\Projects\STM32746G-Discovery\Examples\ADC\ADC_RegularConversion_DMA\MDK-ARM\RTE\Device\STM32F746NGHx\FrameworkCubeMX.gpdsc' is missing
So... what kind of advice could you gave to me to make my project and fix that missing file?
Thanks i wait for your responses!
#fail #bsp #stm32f7 #blinky2015-10-12 7:49 AM
Hi noto.federico,
I don't understand what are you trying to do exactly. Could you please explain when you got this error?-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2015-10-12 11:01 AM
I'm trying to use BSP libraries on Keil, starting a project on STM32CUBEMX. I can't add bsp libraries without getting that error from a missing file. But i done some research and i find out that error is something general, something done on
purpose or not by ST/Keil that makes customer to not be allowed to use BSP libraries and to not be able to start a project in keil and link it with CubeMX. If you keep not understanding i will upload some img later.
Thanks for your reply.2015-10-12 11:15 AM
I'm trying to make blink ld1 from stm32f7 discovery connected through PI1 ( Arduino D13 pin ) using HAL drivers , mounting a base project on STM32CUBEMX and the generating the code on keil, i had no success and having a look on examples i found out that BSP drivers helps a lot to success in my little a silly project.
But when i tried to add those libraries on keil using Manage Run-Time Enviroment , and resolving all the others libraries needed for Basic i/o from BSP just one it isn't resolved and that is the one related to STM32Cube Framework (API) wich any of both displayed options ( Configuration via RTE Device.h and Configuration via STM32CubeMX) fix the problem and in compiling instance that error appearsWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.