2015-03-25 11:20 PM
Hi to all,
I have two stm32f3 discovery with 1 nrf24L01 transceiver on each one. I want to send a packet from one and receive this packet on the other one. Can someone help me? I have no idea. Thanks...2015-03-26 7:54 AM
Hi,
Here is a resource that should help you out, basically you just need to make a SPI connection to the module and issue commands for configuring the module and transmitting and receiving. I believe the resource provides an implementation for SPI and GPIO implementations.http://stm32f4-discovery.com/2014/06/library-17-nrf24l01-stm32f4xx/Thanks,George2015-03-27 1:59 PM
it seems good thanks...
i think i have to change that code to make it campatible with F3, since it is originally for F4. Can you help me on that? I think i have to change the pins, stuff about alternate function...what else? thanks again2015-03-30 7:28 AM
The quickest way to get up in running is to use the Cube middleware, I would suggest using the gpio implementation library that is on that page to get you up and running then migrate the to the SPI version if needed. To migrate the code, you should be able to get away with the .c file as is and change the includes on the .h file to refelect the stm32 f3
#include ''stm32f3xx.h''#include ''stm32f3xx_gpio.h''Then in your defines.h set up the pins you configured in stm32cube for GPIO and you should be up in running.Thanks2015-04-04 12:54 PM
I'm using IAR at the moment. isn't it good enough?
Anyway, i tried the code above, getting the missing library from https://github.com/MaJerle/stm32f429 Some libraries include only .h file, and then call functions defined in the .c file (not included) rather than the included .h with same name. Another library include himself. It seems bad code...2015-04-04 2:15 PM
I'm using IAR at the moment. isn't it good enough?
I'd imagine it's just fine. You might however just want to use the F3 standard peripheral library, and review the SPI support there.2015-10-02 2:23 AM
hi, have you resolved your problem? if yes, can you help me? I have the same problem and I don't know what I have to do.
2015-10-07 6:54 AM
Hi squa.paul,
It should be better to initiate a new discussion in which you describe precisely your problem and in which environment (HW/FW...).-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2015-10-09 8:40 AM
I didn't initiate a new discussion becouse I saw this post from arci.vito that has the same problem I have, with the same HW.
2015-10-09 9:13 AM
So you have two STM32F3-DISCO, with NRF24L01, IAR tools, and no idea what you're doing?
The problem with these types of question is that they're chronically open ended. I think you're going to have to read the related documentation, and look at implementation examples on this, and other, platforms to get a sense of what's required. When you have a specific question about a particular facet of the problem, or why a particular piece of code isn't working, frame it as such.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.