2012-03-02 12:28 PM
Hi, I am trying to update the fash of STM32F407 by using the Flash Loader Demo V1.3, but it does not seem to communicate to my processor. I used this program to flash my STM32F10x series, but I don't know if it will work for F4xx series. Could someone tell me what do I need to update the flash through RS232 interface. Thanks
Nhan Pham #stm32f4xx2012-03-02 4:22 PM
Try v2.4.0 should support the F2, and the F4 is very similar.
2012-03-05 6:45 AM
Hi Clive,
Is there any user manual for this new version. I did assumed its baud rate is the same as older version (57600), Parity = Even, Flow Control = OFF. It doesn't seem to work for me. I did tried several different baud rate but it acts the same. I can see the processor's RX1 activity, but the TX1 just goes high and stay high. By the way, the processor is in the right mode (BOOT0 = 1, BOOT 1 = 0) when power is applied. If you know anything else for me to try, please help. Thanks2012-03-05 11:35 AM
Is there any user manual for this new version. I did assumed its baud rate is the same as older version (57600), Parity = Even, Flow Control = OFF. It doesn't seem to work for me. I did tried several different baud rate but it acts the same. I can see the processor's RX1 activity, but the TX1 just goes high and stay high. By the way, the processor is in the right mode (BOOT0 = 1, BOOT 1 = 0) when power is applied. If you know anything else for me to try, please help. Thanks
It should auto-baud, ie it measures the 0x7F pattern to compute bit timing. As I recall it should also support USART3, and USB connectivity, there is a manual and it covers additional pin states. The USART needs to go to something like a MAX232 to interface to RS232 level signals.
2012-03-06 5:49 AM
Yes, I have an external RS232 transceiver. I moved to UART3 and it works fine. So I guess the new chip does not support UART1.
2012-03-06 5:06 PM
USART1 is supposed to work, I haven't experimented with it, but :
''USART3_RX (PB11), USART3_RX (PC11), CAN2_RX (PB05), OTG_FS_DM (PA11) and OTG_FS_DP (PA12) pins must be kept at a high or low level during the detection phase.''We’re moving the ST Community to a new platform to give you a better and more reliable community experience.