2013-09-11 7:07 PM
Hello,
I have paired up an STM32F4Discovery board with an FT2232H part from FTDI. The purpose of this is to use the CPU-FIFO mode of the FTDI part for faster USB data transfer. I made the necessary modifications to the hardware (ie removed pull-up resistors on shared FSMC signals). I completed a driver and have it working for the most part. Reading data from a PC by the Discovery board works quite well. However, I am having an issue sending data to the PC. All of my bytes make it across, however, for reasons unknown I am always seeing an extra 8 bytes of 0x00 prepended to all my messages. eg [0x00, 0x00, 0x00, 0x00, 0x000x00, 0x00, 0x00, <my data ...>] A little background about the driver:My test program reads a 256 byte payload from the PC and echoes it back. Using a USB analyzer I can see the packets going back to the PC and noticed the extra 8 bytes of 0x00 are prepended to my messages. However, when I single step with the ST-Link I see the correct payload being written to the starting address of 0x60000000. I am hoping this is a configuration issue with my driver. Please see my driver code below.
/* Private define ------------------------------------------------------------*/
#define FT2232H_RAM ((uint32_t)0x60000000) /* Write/Read Enable use the same address as per FT2232H spec sheet*/
/*******************************************************************************
* Function Name : Ft2232hGpioConfig
* Description : Configures FT2232H Control lines (FSMC Pins) in alternate function
Push-Pull mode.
* Input : None
* Output : None
* Return : None
* Attention : None
*******************************************************************************/
void Ft2232hGpioConfig(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
/* Enable GPIOs clock */
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOD | RCC_AHB1Periph_GPIOE , ENABLE);
/* Enable FSMC clock */
RCC_AHB3PeriphClockCmd(RCC_AHB3Periph_FSMC, ENABLE);
/*-- GPIOs Configuration ------------------------------------------------------*/
/*
+-------------------+--------------------+------------------+------------------+
+ SRAM pins assignment +
+-------------------+--------------------+
*/
/* GPIOD configuration */
/* Set PD.00(FSMC_D2), PD.01(FSMC_D3), PD.04(FSMC_NOE), PD.05(FSMC_NWE),
PD.07(FSMC_NE1), PD.11(FSMC_A16), PD.14(FSMC_D0), PD.15(FSMC_D1) as alternate function push pull */
GPIO_PinAFConfig(GPIOD, GPIO_PinSource0, GPIO_AF_FSMC);
GPIO_PinAFConfig(GPIOD, GPIO_PinSource1, GPIO_AF_FSMC);
GPIO_PinAFConfig(GPIOD, GPIO_PinSource4, GPIO_AF_FSMC);
GPIO_PinAFConfig(GPIOD, GPIO_PinSource5, GPIO_AF_FSMC);
GPIO_PinAFConfig(GPIOD, GPIO_PinSource7, GPIO_AF_FSMC);
GPIO_PinAFConfig(GPIOD, GPIO_PinSource11, GPIO_AF_FSMC);
GPIO_PinAFConfig(GPIOD, GPIO_PinSource14, GPIO_AF_FSMC);
GPIO_PinAFConfig(GPIOD, GPIO_PinSource15, GPIO_AF_FSMC);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1 | GPIO_Pin_4 | GPIO_Pin_5 |
GPIO_Pin_7 | GPIO_Pin_11 | GPIO_Pin_14 | GPIO_Pin_15;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; //GPIO_PuPd_DOWN;
GPIO_Init(GPIOD, &GPIO_InitStructure);
/* Set PE.07(FSMC_D4), PE.08(FSMC_D5), PE.09(FSMC_D6), PE.10(FSMC_D7) as alternate function push pull */
/* GPIOE configuration */
GPIO_PinAFConfig(GPIOE, GPIO_PinSource7 , GPIO_AF_FSMC);
GPIO_PinAFConfig(GPIOE, GPIO_PinSource8 , GPIO_AF_FSMC);
GPIO_PinAFConfig(GPIOE, GPIO_PinSource9 , GPIO_AF_FSMC);
GPIO_PinAFConfig(GPIOE, GPIO_PinSource10, GPIO_AF_FSMC);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_7 | GPIO_Pin_8 | GPIO_Pin_9 | GPIO_Pin_10;
GPIO_Init(GPIOE, &GPIO_InitStructure);
}
/*******************************************************************************
* Function Name : Ft2232hInit
* Description : Configures FT2232H FSMC properties
* Input : None
* Output : None
* Return : None
* Attention : None
*******************************************************************************/
void Ft2232hInit(void)
{
FSMC_NORSRAMInitTypeDef FSMC_NORSRAMInitStructure;
FSMC_NORSRAMTimingInitTypeDef p;
/*-- FSMC Configuration ------------------------------------------------------*/
#if 1
p.FSMC_AddressSetupTime = 5;
p.FSMC_AddressHoldTime = 5; // 0;
p.FSMC_DataSetupTime = 5;
p.FSMC_BusTurnAroundDuration = 0;
p.FSMC_CLKDivision = 0;
p.FSMC_DataLatency = 0;
#endif
p.FSMC_AccessMode = FSMC_AccessMode_A;
FSMC_NORSRAMInitStructure.FSMC_Bank = FSMC_Bank1_NORSRAM1;
FSMC_NORSRAMInitStructure.FSMC_DataAddressMux = FSMC_DataAddressMux_Disable; //FSMC_DataAddressMux_Enable;
FSMC_NORSRAMInitStructure.FSMC_MemoryType = FSMC_MemoryType_PSRAM; //FSMC_MemoryType_PSRAM;
FSMC_NORSRAMInitStructure.FSMC_MemoryDataWidth = FSMC_MemoryDataWidth_8b; //FSMC_MemoryDataWidth_16b;
FSMC_NORSRAMInitStructure.FSMC_BurstAccessMode = FSMC_BurstAccessMode_Disable;
FSMC_NORSRAMInitStructure.FSMC_AsynchronousWait = FSMC_AsynchronousWait_Disable;
FSMC_NORSRAMInitStructure.FSMC_WaitSignalPolarity = FSMC_WaitSignalPolarity_Low;
FSMC_NORSRAMInitStructure.FSMC_WrapMode = FSMC_WrapMode_Disable;
FSMC_NORSRAMInitStructure.FSMC_WaitSignalActive = FSMC_WaitSignalActive_BeforeWaitState;
FSMC_NORSRAMInitStructure.FSMC_WriteOperation = FSMC_WriteOperation_Enable;
FSMC_NORSRAMInitStructure.FSMC_WaitSignal = FSMC_WaitSignal_Disable;
FSMC_NORSRAMInitStructure.FSMC_ExtendedMode = FSMC_ExtendedMode_Enable;
FSMC_NORSRAMInitStructure.FSMC_WriteBurst = FSMC_WriteBurst_Disable;
FSMC_NORSRAMInitStructure.FSMC_ReadWriteTimingStruct = &p;
FSMC_NORSRAMInitStructure.FSMC_WriteTimingStruct = &p;
FSMC_NORSRAMInit(&FSMC_NORSRAMInitStructure);
/*!< Enable FSMC Bank1_SRAM2 Bank */
FSMC_NORSRAMCmd(FSMC_Bank1_NORSRAM1, ENABLE);
}
/**
* @brief Writes a Half-word buffer to the FSMC SRAM memory.
* @param pBuffer : pointer to buffer.
* @param WriteAddr : SRAM memory internal address from which the data will be
* written.
* @param NumHalfwordToWrite : number of half-words to write.
* @retval None
*/
void FsmcWriteBuffer(uint8_t* pBuffer, uint32_t WriteAddr, uint32_t NumWordToWrite)
{
for (; NumWordToWrite != 0; NumWordToWrite--) /* while there is data to write */
{
/* Transfer data to the memory */
*(uint8_t *) (FT2232H_RAM + WriteAddr) = *pBuffer++;
/* Increment the address*/
WriteAddr += 1;
}
}
/**
* @brief Reads a block of data from the FSMC SRAM memory.
* @param pBuffer : pointer to the buffer that receives the data read from the
* SRAM memory.
* @param ReadAddr : SRAM memory internal address to read from.
* @param NumHalfwordToRead : number of half-words to read.
* @retval None
*/
void FsmcReadBuffer(uint8_t* pBuffer, uint32_t ReadAddr, uint32_t NumWordToRead)
{
for (; NumWordToRead != 0; NumWordToRead--) /* while there is data to read */
{
/* Read a half-word from the memory */
*pBuffer++ = *(__IO uint8_t*) (FT2232H_RAM + ReadAddr);
/* Increment the address*/
ReadAddr +=1;
}
}
The FsmcWriteBuffer() function is responsible for sending the bytes to the FT2232H.
Any suggestions or feedback would be greatly appreciated. Thank you!
#fsmc
2013-12-27 7:46 AM
Hi MN,
I was planning to do exactly the same thing, except that I was going to use an FT232H instead of the dual FT2232H, so I did a bit of research and found your message. Have you ever found the reason why 8 bytes would be prepended to a message? I have an USB sniffer and a logic analyser and after reading your message I was going to try and find the issue, but I thought I would ask you first and save some time in case you already found the problem.Thanks!VardWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.