2016-10-25 7:47 AM
I am trying to port the ''STemWin_HelloWorld'' example in Applications section of ''STM32F412G-Discovery'' board of ''stm32cube_fw_f4_v1130 '' package.
The code is originally for STM32F412G which uses FSMC peripheral to interface to LCD. I am trying to adapt to STM32F407ZET6. I have chnaged to startup file for my chip as well as the CMSIS file for the 407 family. the clock I brought to same speed as the original example. LED blinking part of this example is runing ok in my new board. But the FSMC part seems not communication with TFT. I just tried by reading some registers of my LCD controller which is having some values by default. but FSMC access always returns 0 in my debugger. I am stuck here. Do we need any chnage in the FSMC code of STM32F412 when the destination is STM32F407? . As far as I can understand the original code uses function names with prefix FMC, but may be because the original code may be from a chip with FMC .Also FMC is only an enhancement of FSMC and many defines of FMC are just like a wrapper over FSMC parameters. Any clues for my problem? #!stm32f4discovery #fsmc #fmc2016-10-25 10:14 AM
Hello,
Looked at it may be helpful for you, to understand how you should configure FSMC to work with an TFT LCD. Regards2016-10-25 11:10 PM
I am referrring to that Note. Note uses 100Pin chip . My chip is 144 pin. Somewhere it says the FSMC in those chips have slight difference. But cant figure out still.
2017-02-19 4:38 PM
I am also using an stm32f407, and I am unable to toggle the Ax pin so that I can write Data to my ili9341 TFT LCD. Can anyone help me out?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.