2021-03-29 6:10 AM
Hi there,
My new STM32F469I-DISCO just arrived I stumbled upon this part in user manual (UM1932):
4.11 Virtual COM port
The serial interface USART3 is directly available as a virtual COM port of the PC connected
to the ST-LINK/V2-1 USB connector CN1. The virtual COM port settings are configured as:
115200 b/s, 8 bits data, no parity, 1 stop bit, no flow control.
So I did a quick test in CubeIDE and enabled USART6 with default settings and just send one char to my USB-Serial Adapter to check on my PC if the char arrives... and it does.
Now I tried the same with USART3. As I plug in the DISCO board via its integrated STLink my Linux system tells me that a new serial device "ttyACM0: USB ACM" . So again I opened a serial terminal on ttyACM0 but no char gets received from the board.
What I am doing wrong? Or is my understanding wrong? Is "USART3" meant to be part of the STM32F103xxx STLInk or is it part of the boards STM32F469xxx?
Solved! Go to Solution.
2021-03-29 6:19 AM
Found a solution to myself:
When I enabled USART3 it enabled the default pins PD8 / PD9 but the lines that go from the STM32F469 to the STLink STM32F103 are PB10 / PB11 which are the alternate pins for USART3. So I enabled PB10 / PB11 as USART3 manually and violá, the char arrives at serial device ttyACM0.
2021-03-29 6:19 AM
Found a solution to myself:
When I enabled USART3 it enabled the default pins PD8 / PD9 but the lines that go from the STM32F469 to the STLink STM32F103 are PB10 / PB11 which are the alternate pins for USART3. So I enabled PB10 / PB11 as USART3 manually and violá, the char arrives at serial device ttyACM0.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.