2022-08-11 2:58 PM
Hi,
I'm struggling to get the CAN working on a project I'm working on with the STM32F446ZET6. With the project below (CastletRestart) i just get a flat line of 3.3V high on the TX line for CAN1, this is being tested in loop back mode, with the TUT_CAN_F446 project the can works (downloaded from a tutorial) in loopback mode, as far as i can see ive replicated everything across but it still isnt working.
Its likely to be something silly and i do apologise for this being the case but i cannot see what ive missed having reviewed the code countless times.
P.s. i am aware the Tutorial project is targeted at a different micro, but the CAN1 ports are the same.
Any advice welcomed, thank you for your time
Chris
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.