STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! how to write data into stm32l5 flash memory

uint64_t write = 0x1111111122222222;HAL_FLASH_Unlock();if(HAL_FLASH_Program(FLASH_TYPEPROGRAM_DOUBLEWORD,0x0807F000,write)==HAL_OK) { HAL_GPIO_WritePin(GPIOG,GPIO_PIN_12,GPIO_PIN_RESET); } HAL_FLASH_Lock();

sra by Associate II
  • 2687 Views
  • 3 replies
  • 0 kudos

When the external 5V power of the STM32H735g-dk board is supplied, intermittently, the initial reset does not work normally.

When the external 5V power of the STM32H735g-dk board is supplied, intermittently, the initial reset does not work normally.​STM32H735g-dk​CubeIDE​Downloading the latest version of CubeIDE and CubeProgrammer does not solve the problem.​​If the initia...

mSH.1 by Associate III
  • 876 Views
  • 0 replies
  • 0 kudos

STM32F446ZET6 - Struggling to get the CAN running

Hi,I'm struggling to get the CAN working on a project I'm working on with the STM32F446ZET6. With the project below (CastletRestart) i just get a flat line of 3.3V high on the TX line for CAN1, this is being tested in loop back mode, with the TUT_CAN...

CBrun.5 by Associate II
  • 693 Views
  • 0 replies
  • 0 kudos

Using OnePulse mode with Repetition Counter on STM32G4 HRTIM

I have an application which I prototyped on an STM32L476. It works fine, but I need to move up to an STM32G4 since I need extra processing power. I am driving the ADCs quite fast (5.35MHz) and need to use HRTIM to get the sampling times right (sampli...

DMcin.11 by Associate II
  • 5049 Views
  • 7 replies
  • 0 kudos

ADC Common-mode range

Hello, I am trying to understand the common-mode range in differential mode - according to the data-sheet, it looks like it is quite narrow:Could you please clarify?We wish to wok with 0 to 2.5 V signals.Thanks.

0693W00000QNGk5QAH.jpg
Sharon by Associate II
  • 4281 Views
  • 9 replies
  • 0 kudos

unique die and device identifier

Hi, STM32 has a unique device identifier and unique die identifier. is there any possibility to read the value of those ids and also to change their value? Thanks

TLit.1 by Associate
  • 1547 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.