2016-10-26 5:11 AM
I'd like to transfer data from STM32F446 MCU to an array of ST1642GW LED drivers efficiently.
Right now, I do so by a soft SPI interface which is limited in speed and consumes too much CPU time. The real challenge as I see it is the synchronous Latch and MOSI transfer. I have 16 clock cycles for data transfer and command at the same time. Is there a possibility to do so by using the standard peripherals, or, even better, use additional DMA? Thanks!We’re moving the ST Community to a new platform to give you a better and more reliable community experience.