STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB OTG CDC Device busy when trying to send

Posted on September 17, 2016 at 15:15 hey guys, so I am using an STM32F411 as an USB device. It's connected via VCOM to a PC. I am using HAL V2.4.1 from19-June-2 In general it works good, but when I quickly connect and disconnect the u...

bm by Associate II
  • 1031 Views
  • 1 replies
  • 0 kudos

DS18B20 1Wire DMA

Posted on October 26, 2016 at 09:31Hi All...i using stm32f103rbt and Ds18B20 temp sensor.i search for hardware peripheral driver that make 1wire independent from cpu but not find any thing useful.i want to read temp from ds18b20 without delay. how i...

amir_lm35 by Associate II
  • 1610 Views
  • 2 replies
  • 0 kudos

L1 low power, not always the same consumption

Posted on October 25, 2016 at 18:06 Hi, In my quest of low power, I'm not that far from my needs but there's still something I don't understand: RTC is clocked by LSI, while SYSclock is clocked by HSI. __HAL_RTC_CL...

JulienD by Senior
  • 885 Views
  • 1 replies
  • 0 kudos

Where to get CoIDE

Posted on October 22, 2016 at 20:25It's strange but http://www.coocox.org/ do not work. Maybe there is a site from which this distribution can be downloaded? Besides http://www.coocox.org/. Thanks.

anton23 by Associate II
  • 1484 Views
  • 2 replies
  • 0 kudos

HAL_TIM_PWM_Stop leaves output pin in undefined state

Posted on October 18, 2016 at 02:28I'm trying to start/stop a PWM signal to an LED (simple test!!). Using HAL_TIM_PWM_Start() starts the PWM output, HAL_TIM_PWM_Stop() stops the PWM but leaves the output in a random state rather than the (expected) ...

I2S full duplex?

Posted on October 25, 2016 at 18:12Hi, I was trying to attach a AK4554 codec to a STM32F091CB using the SPI/I2S interface when I discovered it is half duplex only. I don't want to change to an F4 with an SAI interface if I can help it, as it is over...

STM32L4 STM32Cube 4.14 SDMMC FATFS DMA TX RX hang

Posted on June 12, 2016 at 10:04Hi.FATFS with polling mode is OK(Except TX uderrun error when interrupt).When using DMA, FATFS works OK with TX DMA only. (DMA interrupt priority should be lower than SD interrupt).FATS works OK with RX DMA only.But w...

isjeon by Associate II
  • 1464 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.