2016-03-31 2:00 AM
Hi. I'm trying to get what I've sent from UART4 port GPIOC10 (TX) GPIOC11 (RX). But every time I can't get what I've sent. For example I'm sending 0x10, reading 0x90.
Port settings; Baud = 9600kbps, 8-bit, Even Parity, 1 Stop bit, No hardware flow control Initializing port with;void serial_init(void)
{ GPIO_InitTypeDef g; USART_InitTypeDef u; // GPIOA clk aktif RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE); // UART4 clk aktif RCC_APB1PeriphClockCmd(RCC_APB1Periph_UART4, ENABLE);g.GPIO_Mode = GPIO_Mode_AF;
g.GPIO_OType = GPIO_OType_PP; g.GPIO_PuPd = GPIO_PuPd_UP; g.GPIO_Speed = GPIO_Speed_50MHz; g.GPIO_Pin = GPIO_Pin_10 | GPIO_Pin_11; GPIO_PinAFConfig(GPIOC, GPIO_PinSource10, GPIO_AF_UART4); GPIO_PinAFConfig(GPIOC, GPIO_PinSource11, GPIO_AF_UART4); GPIO_Init(GPIOC, &g); u.USART_BaudRate = 9600; u.USART_HardwareFlowControl = USART_HardwareFlowControl_None; u.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; u.USART_WordLength = USART_WordLength_8b; u.USART_Parity = USART_Parity_Even; u.USART_StopBits = USART_StopBits_1; USART_Init(UART4, &u); USART_ClearFlag(UART4, USART_FLAG_LBD | USART_FLAG_TC | USART_FLAG_RXNE); USART_ClearITPendingBit(UART4, USART_IT_ERR | USART_IT_FE | USART_IT_IDLE | \ USART_IT_LBD | USART_IT_NE | USART_IT_ORE | \ USART_IT_ORE_ER | USART_IT_ORE_RX | \ USART_IT_PE | USART_IT_RXNE | USART_IT_TC | \ USART_IT_TXE); USART_Cmd(UART4, ENABLE); } and testing it with; void test_serial(void) { //int i; USART_SendData(UART4, (uint16_t)0x10); while (USART_GetFlagStatus(UART4, USART_FLAG_TC) != SET); USART_ClearFlag(UART4, USART_FLAG_TC); //for (i = 0; i < 1000; ++i); while (USART_GetFlagStatus(UART4, USART_FLAG_RXNE) != SET); if ((uint8_t)USART_ReceiveData(UART4) == (uint8_t)0x10) { continue; } } I've added for test the //int i; and the //for... lines. Program doesn't reach the continue line.2016-03-31 2:42 AM
You are in fact in 7E1 mode, for 8E1 you would need to set it in 9-bit mode, as the parity is included in the length.
You also need to mask the data register on reads, in this 7-bit mode, mask with 0x7F2016-03-31 2:48 AM
Thanks clive1. So in 9-bit mode, I need 0xFF
2016-03-31 2:53 AM
Yes depending on the width of the variable you put it in. The DR is 16-bit wide at the bus interface.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.