2016-03-30 8:09 AM
Hi,
I like to ask opinion.Currently, in my project, I am using several UART. I connected a logic analyzer on Tx and Rx of one channel. Then in Tx, in random bytes, I saw frame error indicated by extra bit space at the end of a byte. The receiving terminal can recognize bytes with frame error however it looks dirty.At first im operating at high baudrate, but when I lower baudrate to 9600, it still occur.Also I thought, because the port header is near power jack but i proven it not. I use another UART channel in which its header is far from power source and the frame error still occur.I also thought its because of sampling rate, but even if I use already 24MSample per second, frame error still occur.In Rx, the frame error doesnt happen. only in Tx.Any idea what went wrong?Regards,Mike2016-03-31 12:14 AM
I attached screen shot of the logic analyzer capture.
________________ Attachments : frame_error.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0rq&d=%2Fa%2F0X0000000bem%2FemZrkj5qEjxHHwexVpBwhpSjhrPnVuSIrmDySbezhWE&asPdf=false2016-03-31 12:31 AM
Hi,
Im sorry.. Just now I learned the answer to my question.I did not notice that the machine side is sending with parity even and the application is sending without parity.its already resolve.thank you for time.regards,mj2016-03-31 2:49 AM
Hi javier.michael,
Thanks for your contribution and implimenting your feedback after you finding issue. -Hannibal-We’re moving the ST Community to a new platform to give you a better and more reliable community experience.