2018-01-25 7:26 AM
Hello All
I am sorry to disturb you all ; I am trying to fill the lcd structure with the right values but I think I have problem in understanding it
please could you help me ?
and I see that they are flickers on the LCD what could be the problem ?
here the link for the lcd data sheet
https://img.ozdisan.com/ETicaret_Dosya/475075_773619.pdf
here is my test code
void LCD_Config(void){/* LTDC Initialization -------------------------------------------------------*/ /* Polarity configuration */ /* Initialize the horizontal synchronization polarity as active low */ hltdc_F.Init.HSPolarity = LTDC_HSPOLARITY_AL; /* Initialize the vertical synchronization polarity as active low */ hltdc_F.Init.VSPolarity = LTDC_VSPOLARITY_AL; /* Initialize the data enable polarity as active low */ hltdc_F.Init.DEPolarity = LTDC_DEPOLARITY_AL; /* Initialize the pixel clock polarity as input pixel clock */ hltdc_F.Init.PCPolarity = LTDC_PCPOLARITY_IPC; /* Timing configuration */ /* Horizontal synchronization width = Hsync - 1 */ hltdc_F.Init.HorizontalSync = 139;//40; /* Vertical synchronization height =19;// Vsync - 1 */ hltdc_F.Init.VerticalSync = 19; /* Accumulated horizontal back porch = Hsync + HBP - 1 */ hltdc_F.Init.AccumulatedHBP = 160; /* Accumulated vertical back porch = Vsync + VBP - 1 */ hltdc_F.Init.AccumulatedVBP = 20; /* Accumulated active width = Hsync + HBP + Active Width - 1 */ hltdc_F.Init.AccumulatedActiveH = 632; /* Accumulated active height = Vsync + VBP + Active Heigh - 1 */ hltdc_F.Init.AccumulatedActiveW =1340;// 522; /* Total height = Vsync + VBP + Active Heigh + VFP - 1 */ hltdc_F.Init.TotalHeigh = 634;//285; /* Total width = Hsync + HBP + Active Width + HFP - 1 */ hltdc_F.Init.TotalWidth = 1342;//524; //--- /* Initialize the LCD pixel width and pixel height */ hltdc_eval.LayerCfg->ImageWidth = AMPIRE480272_WIDTH; hltdc_eval.LayerCfg->ImageHeight = AMPIRE480272_HEIGHT; /* Configure R,G,B component values for LCD background color */ hltdc_F.Init.Backcolor.Blue = 0; hltdc_F.Init.Backcolor.Green = 0; hltdc_F.Init.Backcolor.Red = 0;hltdc_F.Instance = LTDC;
/* Layer1 Configuration ------------------------------------------------------*/ /* Windowing configuration */ /* In this case all the active display area is used to display a picture then : Horizontal start = horizontal synchronization + Horizontal back porch = 43 Vertical start = vertical synchronization + vertical back porch = 12 Horizontal stop = Horizontal start + window width -1 = 43 + 480 -1 Vertical stop = Vertical start + window height -1 = 12 + 272 -1 */ pLayerCfg.WindowX0 = 0; pLayerCfg.WindowX1 = 1024; pLayerCfg.WindowY0 = 0; pLayerCfg.WindowY1 = 600;Thank you inadvanced
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.