2025-01-23 9:00 AM
Hello..
I am using STM32F429 Disco Board in which I am trying to interface finger print sensor NB65210 of next biometric using spi and I need to read the finger print data I have a example code in which it is reading properly but it is not reading when I configured for myself l, I have selected proper clock, spi pins, Chip select nreset, nawake, the library which ever they have given I have not modified NBdeviceInitializationA it is getting nbok but after that stocking and giving error code for all library function what will the issue can anyone suggest the solution...
2025-01-24 3:55 AM - edited 2025-01-24 3:58 AM
@Abhishek_nr wrote:I have a example code in which it is reading properly but it is not reading when I configured for myself l
So carefully compare & contrast your implementation against the working one.
Have you checked the interface lines with an oscilloscope and/or logic analyser to see what's actually happening on the wires?
@Abhishek_nr wrote:finger print sensor NB65210
Please post a link to its documentation.
Please post your schematic.
See: How to write your question to maximize your chances to find a solution
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.