2019-05-17 1:17 PM
I am trying to modify my own I2C driver (I don't use Cube) - to talk to a BQ32000 device - it's a I2C RTC chip.
The protocol is shown in the picture below.
The protocol to read requires a "restart" after sending the chip's address and sub-address to establish a new "Read Address".
I am trapping the I2C status register to determine which event flags are being sent.
I am capturing the complete I2C stream with a logic analyzer.
When I issue a "restart" (I set the I2C_CR1_START in CR1) - the logic analyzer is showing a new "start bit" being generated but the I2C device does not place the restart address on the bus. In fact, the I2C device will only transmit a stop bit after the restart.
Reading RM0090 (users manual) - the only place it talks about issuing a restart is when addressing "Master Receive" mode - no mention of restart from "Master Transmit" mode.
As a side not, once the restart if activated (set the I2C_CR1_START in CR1) I would expect a SB event followed by an Address event -- neither are issued.
Can someone explain how to generate a restart from Master Transmit mode?
Thanks.
Joe
2019-05-17 2:42 PM
I do not believe the STM32F4 can properly generate a restart under the conditions I described.
Contrary to the protocol stated for the device, I broke the I2C communications into a Write Block followed by a Read Block where each block was terminated with a STOP bit.
The device properly replies so this question can be closed.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.