2016-09-13 4:41 AM
STM32Cube FW_F4 V1.13.0
I have a board using CAN1, CAN2, SPI_1 and SPI_2 All functions work independantly fine CAN1 and CAN2 work in Polling mode and Interrupt mode. SPI_1 and SPI_2 work OK in polling mode using as follows:- HAL_SPI_TransmitReceive(&hspi1, SPI_Data_Wr_ADC1, SPI_Data_Rd_ADC1, 27, 100); // for SPI2 use (&hspi2) CAN1 and CAN2 work OK using as follows:- // (hcan2) for CAN2 hcan1.pTxMsg->StdId = Out_ID; hcan1.pTxMsg->DLC = 8; hcan1.pTxMsg->RTR = CAN_RTR_DATA; hcan1.pTxMsg->IDE = CAN_ID_STD; hcan1.pTxMsg->Data[0] = byte1; hcan1.pTxMsg->Data[1] = byte2; hcan1.pTxMsg->Data[2] = byte3; hcan1.pTxMsg->Data[3] = byte4; hcan1.pTxMsg->Data[4] = byte5; hcan1.pTxMsg->Data[5] = byte6; hcan1.pTxMsg->Data[6] = byte7; hcan1.pTxMsg->Data[7] = byte8; if(HAL_CAN_Transmit_IT(&hcan1) != HAL_OK) { Error_Handler(); // Send my Error } The code works fine until CAN1 transmits an ID greater that 0x03 in StdID which stops SPI_2 from working, SPI_1 continues to work OK, this fault occurs only in CAN1 if CAN2 Transmit is used all works fine. I have not used any debug as not sure if fault is generated by CAN1 and it's effect on SPI_2 Any help would be appreciated. KR John W2016-09-14 6:36 AM
Hi All,
Re:- Corruption of SPI2. I have found my error, my ADC can be configured for 16 or 24 bit. HAL_SPI_TransmitReceive(&hspi1, SPI_Data_Wr_ADC1, SPI_Data_Rd_ADC1, 27, 100); In early days I configured SPI_Data_Wr_ADC1 with 19 byte array, I subsequently went to 24 bit with a 27 byte array and had not extended the array to 27 bytes, with subsequent consequences. It would appear that hcan1.pTxMsg->StdId = Out_ID; wrote data into the end of SPI_Data_Wr_ADC1 array disrupting the ADC. KR John WWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.