2014-07-22 3:31 AM
I have configured the clock for 168 mhz and for tim2 84 mhz , presaclar = 2 and arr = 200
it is showing 4.6 us in stm32f407vgt6...but in stm32f407igt6 it is showing 24 us .....I have checked the system_init actually it is not entering into the if ((RCC->CR & RCC_CR_HSERDY) != RESET) ....to proceed for HSEStatus = (uint32_t)0x01; it is always entering HSEStatus = (uint32_t)0x00; this might be the problem how to solve it....I have referred one link but also didn't give me any success the link is given below: https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2Fcortex_mx_stm32%2FHSE%20can%20not%20be%20ready%20at%20debug&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews=504 I am using coocox please help why it is not enabling the HSE please help2014-07-22 3:52 AM
NOTE:::: I am using PLL to set the clock config is as follows
*============================================================================= *============================================================================= * Supported STM32F4xx device revision | Rev A *----------------------------------------------------------------------------- * System Clock source | PLL (HSE) *----------------------------------------------------------------------------- * SYSCLK(Hz) | 168000000 *----------------------------------------------------------------------------- * HCLK(Hz) | 168000000 *----------------------------------------------------------------------------- * AHB Prescaler | 1 *----------------------------------------------------------------------------- * APB1 Prescaler | 4 *----------------------------------------------------------------------------- * APB2 Prescaler | 2 *----------------------------------------------------------------------------- * HSE Frequency(Hz) | 8000000 *----------------------------------------------------------------------------- * PLL_M | 8 *----------------------------------------------------------------------------- * PLL_N | 336 *----------------------------------------------------------------------------- * PLL_P | 2 *----------------------------------------------------------------------------- * PLL_Q | 7 *----------------------------------------------------------------------------- * PLLI2S_N | NA *----------------------------------------------------------------------------- * PLLI2S_R | NA *----------------------------------------------------------------------------- * I2S input clock | NA *----------------------------------------------------------------------------- * VDD(V) | 3.3 *----------------------------------------------------------------------------- * Main regulator output voltage | Scale1 mode *----------------------------------------------------------------------------- * Flash Latency(WS) | 5 *----------------------------------------------------------------------------- * Prefetch Buffer | OFF *----------------------------------------------------------------------------- * Instruction cache | ON *----------------------------------------------------------------------------- * Data cache | ON *----------------------------------------------------------------------------- *============================================================================= **************2014-07-22 6:27 AM
Ponder why the external crystal would not start?
Not connected properly, electrical characteristics of the circuit are wrong, you have an external source and need to use bypass mode?2014-07-22 11:51 PM
Yes you are right the external crystal oscillator is not connected.....but when I am connecting the external crystal oscillator it is giving error like
Error: Flash driver function execute timeout. I have pasted the schematics for the connection of Exernal crystal oscillator to PH0 and PH1,If I disconnect the resistor R362 which is connected to external oscillator , the code is getting downloaded but it is taking the internal oscillator. And if I connect the R362 then I am not able to dump the code getting error like Error: Flash driver function execute timeout. ________________ Attachments : Untitled.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0jY&d=%2Fa%2F0X0000000bd7%2F9Oe7a84FaUoonqTopjzPPLuCbCQSOAbRq4_2TJ8cprQ&asPdf=false2014-07-23 5:32 AM
If the external clock is 25 MHz, perhaps you should modify the PLL settings to reflect that, and not the 8 MHz settings you have now? Adjust also HSE_VALUE
2014-07-24 3:29 AM
Yes I have done it.........but still the problem exists ...it is still taking the internal oscillator ....Now I am able to connect the external osc by using 200k resistor before I was using 10 k resistor so the code was not dumping now the code is getting dumped by changing it to 200k....
but even after it is connected it is behaving same .. I am not able to see any sine wave across the ext osc.2014-07-24 9:20 PM
please reply
2014-07-24 10:34 PM
Probing it directly is likely to interfere with the characteristics of the circuit, you should be able to look at the HSE and PLL indirectly via the MCO pin (PA8) and configuring that to output internal clock signals.
You can also run the part from the HSI (16 MHz), and PLL clocks generated from the HSI. You need to evaluate why the HSE isn't starting properly. You want to look at the component values and specs, an how the circuit is laid out. Confirm the capacitors are the correct values. HC-49S-C16QSA-25Mhttp://search.alkon.net/cgi-bin/pdf.pl?pdfname=05616.pdf
-20 to +70 C 16pF Load Capacitance Frequency Tolerance +/-20*10-6 Frequency Stability +/- 30*10-6 AT Fundamental 25 MHz CC0603JRNPO9BN200Yageo Multilayer Ceramic Capacitors MLCC - SMD/SMT 20PF 50V 5% 0603</span>
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.