2025-06-05 12:26 AM
Hello, I am currently creating an inverter using STMC Board Designer, the MCU is STM32F407IGT6,the clock source is internal clock, here are some screenshots of my configuration, it was working fine until the inverter was generated successfully, and when I have everything ready to create the program, I get an error as shown in the picture below.I have version 6.4.0.I'm desperate to know why I'm getting this error, thanks.
Best regards.
{
"type": "inverter",
"contentVersion": "1.0",
"descVersion": 5,
"name": "F407_72V300A_New",
"PN": "F407_72V300A_New",
"algorithmCompatibility": [
"FOC"
],
"mcu": "STM32F407IGTx",
"clockFrequency": 168,
"motorDrives": [
{
"name": "M1",
"minRatedVoltage": 10,
"maxRatedVoltage": 100,
"maxRatedCurrent": 300,
"features": [
{
"type": "CurrentSensing",
"name": "CurrentSensing",
"tRise": 1,
"hwVariants": [
{
"signals": {
"CURRENT_ICS_U": [
{
"name": "PC2",
"help": {},
"cost": 0
}
],
"CURRENT_ICS_V": [
{
"name": "PC3",
"help": {},
"cost": 0
}
]
},
"type": "TwoICSCurrents",
"cost": 0,
"icsGain": 0.0044
}
]
},
{
"type": "PhaseVoltageGeneration",
"name": "PhaseVoltageGeneration",
"hwVariants": [
{
"signals": {
"PWM_CHU_H": [
{
"name": "PA8",
"help": {},
"cost": 0
}
],
"PWM_CHV_H": [
{
"name": "PA9",
"help": {},
"cost": 0
}
],
"PWM_CHW_H": [
{
"name": "PA10",
"help": {},
"cost": 0
}
],
"PWM_CHU_L": [
{
"name": "PA7",
"help": {},
"cost": 0
}
],
"PWM_CHV_L": [
{
"name": "PB0",
"help": {},
"cost": 0
}
],
"PWM_CHW_L": [
{
"name": "PB1",
"help": {},
"cost": 0
}
]
},
"type": "DrivingHighAndLowSides",
"cost": 0,
"deadTime": 3000,
"highSideSwitchesDrivingPolarity": "Active high",
"lowSideSwitchesDrivingPolarity": "Active high"
}
],
"driverPN": "L6230",
"driverName": "L6230",
"tNoise": 1000,
"maxSwitchingFreq": 30,
"minDeadTime": 100
}
]
}
],
"clockSource": "internal_osc",
"features": []
}
Solved! Go to Solution.
2025-06-05 11:06 PM
Hello @iskan,
Thank you for the report. The issue comes from that Clock Source=Internal RC Oscillator is not supported by the Workbench for STM32F4 series (to be solved on next release).
Selecting External Crystal clock as Clock Source should solve the issue.
2025-06-05 11:06 PM
Hello @iskan,
Thank you for the report. The issue comes from that Clock Source=Internal RC Oscillator is not supported by the Workbench for STM32F4 series (to be solved on next release).
Selecting External Crystal clock as Clock Source should solve the issue.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.