2017-04-12 9:44 PM
Dear Sir,
I m using timer1 of STM32F407 to get Edge-aligned PWM & using the following settings to give 84 MHz clock to timer1 :
RCC->PLLCFGR &= ~(0x1F); //PLLM=0
RCC->PLLCFGR |= 0x08; //PLLM=8 RCC->PLLCFGR &= ~(0x7FC0); //PLLN=0 RCC->PLLCFGR |= (84)<<6; //PLLN=84 RCC->PLLCFGR |= 0x010000; //PLLP=4 RCC->PLLCFGR |=(4)<<24; //PLLQ=4 RCC->CR |= RCC_CR_PLLON; while((RCC->CR & RCC_CR_PLLRDY)==0); //stay here if PLL not ready RCC->CFGR |= 0x0000002; // PLL selected as system clockBasic steps followed:
1. HSI internal (16 MHz) is chosen as oscillator.
2. PLLM is set to 8.
3. PLLN is set to 84.
4. PLLP is set to 4.
5. PLL is switched ON.
6. PLL is checked whether it is locked properly.
7. System clock input source MUX selects PLL as input.
8. PPRE2;PPRE1;HPRE in RCC_CFGR register are left to their default values.
As per my application, i need PWM frequency more than 16 MHz. Which i m not getting even after entering these settings. Even this 16 MHz PWM is not stable enough. Please! provide the required correction.
2017-04-13 1:45 AM
Hi
GUPTA.NEERAJ
,I'd highly recommend you to start from Timerexamples under the
STM32F4xx_DSP_StdPeriph_Lib_V1.8.0\Project\STM32F4xx_StdPeriph_Examples\TIM, it can be very useful.-Nesrine-
2017-04-13 2:32 AM
At high frequencies you'll need to select a PLL clock that is cleanly divisible by the output clock you want. For 16 MHz try 128 MHz
2017-04-13 4:09 AM
Hi Nesrine M,
i have already completed this exercise as mentioned by you using
STM32F4xx_DSP_StdPeriph_Lib_V1.8.0
.I have also generated the required code using STM32 CUBE MX. But still the result is same. Please! provide the required corrections .
2017-04-13 6:10 AM
Dear Clive,
i m able to achieve upto 16 MHz using PLL clock as advised by you. But my requirement dictates PWM frequency > 16 MHz. I m not able to go above this frequency. Please! advise to how achieve this.
2017-04-13 7:59 AM
I'm saying the PLL clock needs to be an integer multiple, as the TIM can only do integer division
If you clock the PLL/CPU at 168 MHz, you could get a 21 MHz or 42 MHz PWM signal, but you won't be able to have much control of the pulse width due to the small number involved.
ie If you divide the TIMCLK by 4, you options would by a duty cycle of 0%, 25%, 50% and 75%
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.