2017-03-20 7:53 AM
Hi,
In my application I'm using the Independent watchdog on a STM32F407 with a maximum reload period of 2 ms. During some maintenance operations, we need to save some configuration parameters in flash memory. Even if we use the 16 kB sector, the erase time is greater than 2 ms and the IWDG make the MCU reset. Because there is only on flash bank on the 407 I can't kick the watchdog during the flash erase operation (and the bus stalls anyway), and it is not possible to disable the IWDG.
In order to avoid these resets, I tried to reconfigure the IWDG with a max reload period of a few seconds which is, I measured, way greater than the time needed for the erase operation.
In debug, the registers of the IWDG looks fine after the reconfiguration but when I tried in release or in debug but with no break point near the erase sector routine I have a IWDG reset.
Is there any way to avoid this behavior or am I just not correctly reconfiguring the IWDG ?
Many thanks in advance,
Pablo
Solved! Go to Solution.
2017-03-24 3:42 AM
To completely safe we need to check for PVU and RVU to be reset before writing them.
The following code seems to work :
while((IWDG->SR & IWDG_SR_RVU != 0) || (IWDG->SR & IWDG_SR_PVU != 0))
{
// Continue to kick the dog
IWDG_ReloadCounter();
}
// Unlock register
IWDG_WriteAccessCmd(IWDG_WriteAccess_Enable);
// Update configuration
IWDG_SetReload(reload);
IWDG_SetPrescaler(prescal);
// Wait for the new configuration to be taken into account
while((IWDG->SR & IWDG_SR_RVU != 0) || (IWDG->SR & IWDG_SR_PVU != 0))
{
// Continue to kick the dog
IWDG_ReloadCounter();
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
Thanks a lot for your answers !
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.