2016-05-18 8:52 AM
Hi,
I can't get the GPIO into high speed as stated in data sheet 42Mhz with the following code even I already set the clock to Max based on Internal clock:RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE);GPIO_InitDef.GPIO_Pin = GPIO_Pin_2;GPIO_InitDef.GPIO_OType = GPIO_OType_PP;GPIO_InitDef.GPIO_Mode = GPIO_Mode_OUT;GPIO_InitDef.GPIO_PuPd = GPIO_PuPd_NOPULL;GPIO_InitDef.GPIO_Speed = GPIO_Speed_100MHz;//initialisation port B pinsGPIO_Init(GPIOA, &GPIO_InitDef);while(1){ GPIOB->BSRRL = GPIO_Pin_2; GPIOB->BSRRH = GPIO_Pin_2;}When I hooked the pin to theoscilloscope it only
show
14Mhz, is the instruction cycle too slow to achieve 42Mhz or is the GPIO characteristic issue (rising and falling time)?
Clock setting is based on following SetSysClockInternal() function, Clock parameters setting:static void SetSysClockInternal(void){ // HSI_RC = 16Mhz // SYSCLK = 168Mhz // HCLK = 168Mhz // APB1 peripheral = 42Mhz // APB1 timer = 84Mhz // APB2 peripheral = 84Mhz // APB2 timer = 168Mhz __IO uint32_t HSIStatus = 0; /* Enable HSI */ RCC->CR |= ((uint32_t)RCC_CR_HSION); /* Wait till HSI is ready and if Time out is reached exit */ do { HSIStatus = RCC->CR & RCC_CR_HSIRDY; } while(HSIStatus == 0); /* Select regulator voltage output Scale 1 mode, System frequency up to 168 MHz */ RCC->APB1ENR |= RCC_APB1ENR_PWREN; PWR->CR |= PWR_CR_VOS; /* HCLK = SYSCLK / 1*/ RCC->CFGR |= RCC_CFGR_HPRE_DIV1; /* PCLK2 = HCLK / 2*/ RCC->CFGR |= RCC_CFGR_PPRE2_DIV2; /* PCLK1 = HCLK / 4*/ RCC->CFGR |= RCC_CFGR_PPRE1_DIV4; /* Configure the main PLL */ RCC->PLLCFGR = PLL_M | (PLL_N << 6) | (((PLL_P >> 1) -1) << 16) | (RCC_PLLCFGR_PLLSRC_HSI) | (PLL_Q << 24); /* Enable the main PLL */ RCC->CR |= RCC_CR_PLLON; /* Wait till the main PLL is ready */ while((RCC->CR & RCC_CR_PLLRDY) == 0) { } /* Configure Flash prefetch, Instruction cache, Data cache and wait state */ FLASH->ACR = FLASH_ACR_ICEN |FLASH_ACR_DCEN |FLASH_ACR_LATENCY_5WS; /* Select the main PLL as system clock source */ RCC->CFGR &= (uint32_t)((uint32_t)~(RCC_CFGR_SW)); RCC->CFGR |= RCC_CFGR_SW_PLL; /* Wait till the main PLL is used as system clock source */ while ((RCC->CFGR & (uint32_t)RCC_CFGR_SWS ) != RCC_CFGR_SWS_PLL); { }}regards,David #stm32 #internal-clock #gpio2016-05-18 9:27 AM
Hi david.zhanwey,
You are configuring GPIOA and toggling the GPIOB !?-Hannibal-2016-05-18 9:51 AM
But what does that actually assemble to? Do you have optimization on? Which compiler?
This whole thing has been discussed here previously, and I'm pretty sure I can get that number well north of 14 MHz if coded efficiently.This is a poor strategy to get high speed signalling, suggest if you want 42 MHz, use a timer.2016-05-18 6:32 PM
Hi Hannibal,
Thank for your reply.Sorry for the mistake, I am configuring GPIOA and toggling GPIOA.RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE);GPIO_InitDef.GPIO_Pin = GPIO_Pin_2;GPIO_InitDef.GPIO_OType = GPIO_OType_PP;GPIO_InitDef.GPIO_Mode = GPIO_Mode_OUT;GPIO_InitDef.GPIO_PuPd = GPIO_PuPd_NOPULL;GPIO_InitDef.GPIO_Speed = GPIO_Speed_100MHz;//initialisation port B pinsGPIO_Init(GPIOA, &GPIO_InitDef);while(1){ GPIOA->BSRRL = GPIO_Pin_2; GPIOA->BSRRH = GPIO_Pin_2;}regards,ZW Siew2016-05-18 6:37 PM
Hi clive1,
I am using CoIDE with optimizate Most (-O3).My intention is to test the toggling speed as fast as possible, timer interrupt handle will waste some instruction cycles. That why I put it into main loop.thank,regards,ZW Siew2016-05-19 10:08 PM
Not all compilers are equal.
When i started to play with MCU, i was using atolic, it was just horrible even with best optimization. Tests showed me ( gpio toggling and math) that IAR ARM same code make as much as 20x faster, with atolic i was never get more than fev MHz toggling, while with IAR ARM i always get sysclk/2We’re moving the ST Community to a new platform to give you a better and more reliable community experience.