2014-12-23 6:36 AM
Hi,
I've been using the STM32F4 discovery kit (the one that contains the STM32F407 MCU) and I've noticed something strange. When I stopped the code at the SystemInit fuction and probed the HSE I saw that it was already oscillating although it hasn't been activated by software yet (I tried all the code lines before the SetSysClock function and I tried manually disabling the HSE). Could someone explain this behavior? Thanks in advance2014-12-23 9:53 AM
Where exactly are you probing it? Because there is an 8 MHz signal delivered by the ST-LINK's F103 part to a point very close to the XTAL. A lot of other DISCO boards don't have an HSE crystal and have solder bridges, or zero ohm, connectivity to the MCO signal.
2014-12-23 11:40 PM
I'm probing C14 and C15 (next to X2), they are all mounted (including R24 & R25).
I've made sure that SB13 & SB14 are not connected so I'm pretty sure I'm measuring the X2 crystal and not the external oscillator.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.