2021-07-04 5:30 PM
I have trie everything i am able to upgrade firmware to erase device to see it in win 10 but when i try to flash something i receive program errore 0x08000000! and flash is completely empy. I have he board monunted over a PCD that i do not know why took fire but the STM32F407 is not touched by fire and i immediatly shoot down infact i see led connection and file system i cannot flash it.
02:23:47 : ST-LINK SN : XXXXXXXXXX
02:23:47 : V2J37M26
02:23:47 : Connected via SWD.
02:23:47 : SWD Frequency = 4,0 MHz.
02:23:47 : Connection mode : Normal.
02:23:47 : Debug in Low Power mode enabled.
02:23:47 : Device ID:0x413
02:23:47 : Device family :STM32F405xx/F407xx/F415xx/F417xx
02:23:59 : Flash memory erased.
02:24:22 : Programming error @ 0x08000000!
02:24:24 : Programmed memory Checksum: 0x00000000
02:24:25 : Flash memory [0x08000000:0x0BFFFC00] Checksum: 0x00000000
2021-07-04 11:29 PM
Hello @MBezz.1 ,
I honestly didn't understand a lot what you wrote, but there's is a strong probability that the chip is fried or at least some solder joints are bad.
Best regards,
@SBEN .2
2021-07-05 8:29 AM
Sorry i am a noob in STM32 I try to better explain i have mounted STM32F407 Discovery Board over a custom board assembled by me and a specific component of this custom board took fire , with no evident damage on STM32F407 Discovery Board . i have immediately stop current flow and now with st Link i am able tof ully erase chip and the board is recognized by both ST-LINK and STM32CubeProgrammer but i am not able to flash any bin program because i receive the error of the topic. But i can upgrade and downgrade board firmware. Windows drivers work with no problem. Flash memory at 0x08000000 is always empty with Checksum: 0x00000000
2021-07-05 10:33 AM
The firmware on the ST-LINK (STM32F103) is independent from the F407
2021-07-05 4:06 PM
so if i have understod you belive that only STM32F103 is ok while STM32F407 is broken but both erase and all zero read is good , well it can be a signal of no response ,could be a good idea to desolder and resolder STM32F407 ?
2021-07-05 11:37 PM
Hello @MBezz.1 ,
Maybe try replacing the chip altogether.
Best regards,
@SBEN .2
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.