2021-01-04 2:25 PM
Hello All,
I am trying to get eeprom emulation working on a stm32f405RG**.
I created a new simple project in STM32CubeIde using the eeprom code from the stm32f4cubeide packages. specifically I am using the code from STM32Cube_FW_F4_V1.25.0\Projects\STM32F401RE-Nucleo\Applications\EEPROM\EEPROM_Emulation
however I keep getting an error from the EE_Init() function below:
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* Unlock the Flash Program Erase controller */
HAL_FLASH_Unlock();
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
//MX_SPI2_Init();
//MX_TIM3_Init();
//MX_SPI3_Init();
//MX_TIM4_Init();
//MX_TIM5_Init();
//MX_TIM8_Init();
//MX_USART3_UART_Init();
//MX_TIM2_Init();
//MX_ADC1_Init();
//MX_USART1_UART_Init();
/* USER CODE BEGIN 2 */
/* EEPROM Init */
if( EE_Init() != EE_OK)
{
Error_Handler();
}I setup my virtual addresses the same as in the example:
uint16_t VirtAddVarTab[NB_OF_VAR] = {0x5555, 0x6666, 0x7777};
uint16_t VarDataTab[NB_OF_VAR] = {0, 0, 0};
uint16_t VarValue,VarDataTmp = 0;I suspect it could be a problem because the code was made for STM32F401RE. But I think it should be similar....
Any Ideas or help would be appreciated.
Thanks,
Trevor
2021-01-05 2:16 AM
What is the error code? If you debug-step into EE_Init(), do you see what causes the error? When you ported to the other chip: did you check RAM+Flash sizes and layout in the linker file?
2021-01-05 11:03 AM
Hi KnarfB,
Here is my linker file MEMORY layout (STM32F405RGTX_FLASH.ld):
MEMORY
{
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 128K
CCMRAM (rw) : ORIGIN = 0x10000000, LENGTH = 64K
FLASH_BOOT (rx) : ORIGIN = 0x8000000, LENGTH = 32k
EMULATED_EEPROM (rwx) : ORIGIN = ORIGIN(FLASH_BOOT) + LENGTH(FLASH_BOOT), LENGTH = 32k
FLASH (rx) : ORIGIN = ORIGIN(EMULATED_EEPROM) + LENGTH(EMULATED_EEPROM), LENGTH = 1024k - LENGTH(FLASH_BOOT) - LENGTH(EMULATED_EEPROM)
}EE_Init() is returning 128(dec) (PAGE_FULL), line 22 in the below snippit:
else /* Page0 valid, Page1 receive */
{
/* Transfer data from Page0 to Page1 */
for (VarIdx = 0; VarIdx < NB_OF_VAR; VarIdx++)
{
if ((*(__IO uint16_t*)(PAGE1_BASE_ADDRESS + 6)) == VirtAddVarTab[VarIdx])
{
x = VarIdx;
}
if (VarIdx != x)
{
/* Read the last variables' updates */
ReadStatus = EE_ReadVariable(VirtAddVarTab[VarIdx], &DataVar);
/* In case variable corresponding to the virtual address was found */
if (ReadStatus != 0x1)
{
/* Transfer the variable to the Page1 */
EepromStatus = EE_VerifyPageFullWriteVariable(VirtAddVarTab[VarIdx], DataVar);
/* If program operation was failed, a Flash error code is returned */
if (EepromStatus != HAL_OK)
{
return EepromStatus;
}
}
}
}In main.c, flashunlock is HAL_OK. which seems to mean the flash is unlocked.
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* Unlock the Flash Program Erase controller */
HAL_StatusTypeDef flashunlock = HAL_FLASH_Unlock();
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
//MX_SPI2_Init();
2021-01-05 2:36 PM
It looks like I was using to large of values (from the example 0x5555, 0x6666, 0x7777) for the virtual addresses. using virtual address 0x0,0x1,0x2, etc seems to be working for me.
2021-01-07 12:37 PM
UPDATE: The Above is really not the correct solution to the problem. I believe I am still getting errors.
To be clear I am trying to get eeprom emulation working on the both the f4 (above) and a stm32H7. right now I am working with the H7 again and am having trouble with the EE_VerifyPageFullWriteVariable function:
/* Check each active page address starting from begining */
while (Address < PageEndAddress)
{
/* Verify if Address and Address+2 contents are 0xFFFFFFFF */
__IO uint32_t* addressAsPointer = Address;
uint32_t addressValue = (*addressAsPointer);
if (addressValue == 0xFFFFFFFF)
{
/* Set variable data */
FlashStatus = HAL_FLASH_Program(FLASH_TYPEPROGRAM_FLASHWORD, Address, ((uint32_t)data32));
/* If program operation was failed, a Flash error code is returned */
if (FlashStatus != HAL_OK)
{
return FlashStatus;
}
/* Set variable virtual address */
FlashStatus = HAL_FLASH_Program(FLASH_TYPEPROGRAM_FLASHWORD, Address + 32, ((uint32_t)VirtAddress1));
/* Return program operation status */
return FlashStatus;
}
else
{I get a hardfault when dereferencing the addressAsPointer variable. the address seems valid (its in flash range 0x81cb680) and the value is even extracted into the addressValue variable. non-theless I get a hardfault
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.