2021-01-07 9:20 AM
the problem is that When I define the arrays like this :
float Data_Set_X[15000];
float Data_Set_Y[15000];
float Data_Set_Z[15000];
I get the RAM overflow error which is: `.bss' will not fit in region `RAM' Timer-Blink-Test_CM7 C/C++ Problem
when I initilaze at least one of the arrays or three of them , the error will be disappeared.
float Data_Set_X[15000]={0};
float Data_Set_Y[15000];
float Data_Set_Z[15000];
in linker script file it is written that:
/* Specify the memory areas */
MEMORY
{
RAM_EXEC (rx) : ORIGIN = 0x24000000, LENGTH = 256K
RAM (xrw) : ORIGIN = 0x24040000, LENGTH = 256K
}
/* The startup code goes first into RAM_EXEC */
/* The program code and other data goes into RAM_EXEC */
/* Constant data goes into RAM_EXEC */
/* Initialized data sections goes into RAM, load LMA copy after code */
and there is a separated part of the RAM for /* Uninitialized data section */ according to the linker script.
the RAM size is 1MB and around 800KB is accessible for the user. MCU has dual core and I use the M7 Core. this core can access to a 512KB RAM area as it is mentioned in the Linker Script file. the whole size of these three arrays are 180KB
I have attached the linker script file to this message.
Thank you!
2021-01-07 10:24 AM
Accoding to your .ld file: Uninitialized data goes to .bss, initialized global data finally goes to .data. Actually, initialized global data is copied from RAM_EXEC to RAM at startup before entering main. This copying makes more sense for a (persistent) FLASH and I wonder why this RAM to RAM copying is done at all.
Edit: this might be helpful https://interrupt.memfault.com/blog/how-to-write-linker-scripts-for-firmware
2021-01-07 10:34 AM
Related
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.