2018-09-13 1:31 AM
in stm32f4xx_ll_utils.c
__STATIC_INLINE void LL_InitTick(uint32_t HCLKFrequency, uint32_t Ticks)
{
/* Configure the SysTick to have interrupt in 1ms time base */
SysTick->LOAD = (uint32_t)((HCLKFrequency / Ticks) - 1UL); /* set reload register */
SysTick->VAL = 0UL; /* Load the SysTick Counter Value */
SysTick->CTRL = SysTick_CTRL_CLKSOURCE_Msk |
SysTick_CTRL_ENABLE_Msk; /* Enable the Systick Timer */
}
No SysTick IRQ after executing
�?re there any new improved versions of LL files?
2018-09-13 3:04 AM
> No SysTick IRQ after executing
How do you know?
JW
2018-09-14 6:07 AM
because if I use SysTick_Config from core_cm4.h instead LL_InitTick , then SysTick IRQ begin works. Therefore, there is a problem in the LL library.
__STATIC_INLINE uint32_t SysTick_Config(uint32_t ticks)
{
if ((ticks - 1UL) > SysTick_LOAD_RELOAD_Msk)
{
return (1UL); /* Reload value impossible */
}
SysTick->LOAD = (uint32_t)(ticks - 1UL); /* set reload register */
NVIC_SetPriority (SysTick_IRQn, (1UL << __NVIC_PRIO_BITS) - 1UL); /* set Priority for Systick Interrupt */
SysTick->VAL = 0UL; /* Load the SysTick Counter Value */
SysTick->CTRL = SysTick_CTRL_CLKSOURCE_Msk |
SysTick_CTRL_TICKINT_Msk |
SysTick_CTRL_ENABLE_Msk; /* Enable SysTick IRQ and SysTick Timer */
return (0UL); /* Function successful */
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.